Part Number: UCC28C53-Q1 Other Parts Discussed in Thread: UCC28C53 , UCC28C52 Tool/software: Could you pls help with calculation for soft start from the primary (controlling Cs Pin) and secondary (zenor diode and capacitor, slow vout rise)?
We r looking…
Part Number: UCC28C53-Q1 Other Parts Discussed in Thread: UCC28C53
Tool/software:
Hello,
In our project we need isolated no-opto flyback supply.
Our specs shall be,
Vin :18-150V
Vout :15V Iout : 3A
Is UCC28C53-Q1 IC the most up-to-date PWM…
Part Number: UCC28C53-Q1 Tool/software: Hi Ti team,
In UCC28C53-Q1 the minimum operation VDD supply voltage is not specified. What is the minimum operating supply voltage with meeting all operating performance requirements..
I will be using…
Part Number: UCC28C53-Q1 Other Parts Discussed in Thread: PMP30183 , UCC28C53 Tool/software:
Dear Ti team,
I am looking to use UCC28C53-Q1 as a controller for two-switch forward converter. But i want the overcurrent and overvoltage protection feature…
Part Number: UCC28C53-Q1 Tool/software: Hi,
I built a simulation for Boost in Qspice using UCC28C53 and UCC28C53-Q1 PSpice Model ( SLUM838.ZIP).
Even when I ground the COMP pin I still observe some duty cycle in the controller's output.
It seems…
Part Number: UCC28C53-Q1 Other Parts Discussed in Thread: UCC28C53 Tool/software: Hi Team,
Do you have any Calculation sheets or Design guides for choosing or designing the transformer?
For the design requirement,
I/P = 24V
O/P = 5A, 24V
…
Part Number: UCC28C53-Q1 Dear Team,
I am designing the flyback the with Vin 67 to 180rms, and Vo 12V, 2A. I have gone thru the Webench schematic, observed that 18V zener connected across VDD pin for protecting the IC.
the D12 is VZ 18V @ IZT 7mA…
Part Number: UCC28C53-Q1 Other Parts Discussed in Thread: UCC28C56H Tool/software: Dear Team ,
in the EVB of the UCC28C56H Q1, we can see the Short circuit to Ground waveforms. I have some qtns on that pls reply :
1. Does the UCC28Cxx family supports…
Part Number: UCC28C53-Q1 Other Parts Discussed in Thread: TIDA-01505 Hi Experts,
Could you share the reference design for this requirements? Thanks.
1. Input voltage: 150-900V, Output voltage: 14V, Output current: 3A
2. Topology: Flyback, secondary…