Part Number: UCC28C54 Other Parts Discussed in Thread: UCC28C42
As shown in the figure above, when I used UCC28C54 for simulation, the following error occurred. May I ask what caused it?
Part Number: UCC28C54 Other Parts Discussed in Thread: UC2844 , UCC28C44 , TL431 Hi Teams,
What's this resistor's function? Can the converter work without this resistor?
How to design this resistor's value?
BRS,
Marsh
Part Number: UCC28C54 Hi
I encountered a question when promote UCC28C54.
What 20V VDD use external LDO for?
Why can 30V VDD eliminate use of external LDO?
BRs,
Kian
Any single output 8-pin general purpose PWM can be used to design this low power flyback converter. A popular choice might be UCC28C54 . Also, download and use TI Power Stage Designer to help understand different topologies including flyback and more.
…
Hi Sateesh Thanks for the info. I am pleased to see that you have fiiiiiiiiiinally realized that Webench is incorrect. Please have a look at my other posts on the topic of the UCC28C54 and Webench design, as there are many more parts that are totally wrong…
Part Number: WEBENCH-POWER-DESIGNER Other Parts Discussed in Thread: UCC28C54
Hi
I have a WeBench related question regarding a design that WeBench made and how WeBench performs the calculation of turns ratio for a flyback transformer. It concerns a design…
Other Parts Discussed in Thread: UCC28C54 I noticed that the time scale displays in nS not mS. I have attached the "Run to Time Settings set to 50mS (Settings 2). The initial units displays 1000nS (Settings1). I simulated a simple circuit (Circuit 1) with…
Part Number: UCC28C53 Other Parts Discussed in Thread: UCC28C55 , , UCC2800 , UCC28C54 Hi
I have design SMPS using UCC28C55 . I am start designing one solution on below both requirement. I have done schematic and also attached please review and comment. …
Hello Max,
Thank you for your interest in the LM5023 quasi-resonant (QR) flyback controller.
The LM5023 is specifically designed to operate only in QR and DCM modes. It is not possible to configure this controller into CCM operation.
I suggest that you…