Part Number: UCC28C55 Tool/software: Hello,
I am using the UCC28C55 flyback IC.
I am working with voltage mode control and with DCM. Do i need to use the slope compensation circuit?
Thank you
Maor M.
Part Number: UCC28C55-Q1 Tool/software: Hi Ti Team,
I am using UCC28C55-Q1 in my DC-DC converter.
I am using VREF 5V to supply protection circuit of my internal circuit.
If i pull-down COMP pin with MOSFET during some fault condition.Still…
Part Number: UCC28C55-Q1 Other Parts Discussed in Thread: UC2842 Tool/software: Hi TI team,
i am working on UCC28C55-Q1 and I have query regarding how to calculate Rss,Css based on soft start time .It is mentioned in the datasheet as 1mA of the Error…
Part Number: UCC28C55 Tool/software: Hello,
I am using the UCC28C55 is. In the RT pin i placed RT=17.4kOhm and CT=1nF. From the graph i should get 100kHz but i get 50kHz. Why is that?
Thank you
Part Number: UCC28C55-Q1 Other Parts Discussed in Thread: UCC28C55 , Tool/software: I have an isolated 24Vin / 250Vout dc/dc design based on Webench with parameters shown below, and PDF attached. (TI Webench) 24Vin, 250Vout (25W) iso boost converter design…
Part Number: UCC28C55-Q1 Tool/software: Hi Team,
I am designing an isolated DC-DC flyback converter using the UCC28C55-Q1 IC (schematics attached). The Webench Power Designer suggests including an isolation capacitor between the primary and secondary…
Part Number: UCC28C55 Tool/software: Hi Team,
I would like to know if it is possible to use two isolation regulators on the input side to distribute the regulator load while maintaining the isolation requirements.
Thanks,
Mukesh
Part Number: UCC28C55-Q1 Tool/software: Hi.
I'm currently looking into UCC28C55-Q1. There are design which use both primary side regulation (PSR) and secondary side regulation (SSR).
I know that in PSR the regulation and transient response is worse…
Part Number: UCC28C55-Q1 Other Parts Discussed in Thread: UCC28C43 Tool/software: Hi Ti team,
i am doing stability simulation for dc-dc converter by using UCC28C55-Q1 controller in PSICE,but only UCC28C55-Q1 transient model is avaliable in the Ti site…