Part Number: UCC28C59-Q1 Other Parts Discussed in Thread: UCC28C59 , UCC28C43 Tool/software: I'm encountering several critical issues with the Spice model provided by the manufacturer:
VDD Voltage Discrepancy: The expected start threshold is 16V,…
Part Number: UCC28C59-Q1 Tool/software: I'm encountering several critical issues with the Spice model provided by the manufacturer:
VDD Voltage Discrepancy: The expected start threshold is 16V, but the model shows 22µV.
Current Discrepancy: The…
Part Number: UCC28C58-Q1 Other Parts Discussed in Thread: UCC28C56H , UCC28C59 , UCC28C57H Tool/software: Hello,
I have a customer working on a power supply for a new project and we were hoping to get your team's guidance on implementation recommendations…
Part Number: UCC28740 Other Parts Discussed in Thread: UCC28704 , UCC21550 , UCC24610 , UCC24612 , UCC28C59 Tool/software: Hi Team,
Do we have device like INN3649C? Customer requirements are efficiency(>88%) and internal power FET to do high voltage…
Part Number: UCC28C43-Q1 Other Parts Discussed in Thread: UCC28C43 , UCC28C53 , UCC28C59 Tool/software: I've been trying to simulate the design provided by the manufacturer, but I'm encountering issues. The output is consistently zero, although the feedback…
Hello Hailey,
Thank you for reaching out.
Since each output is 1A, is the total power of the system 15.2W? If so, I would recommend the UCC28C59 in a flyback with multiple outputs. This product also has many variations (such as an automotive equivalent…
Part Number: UCC28C58 Tool/software: Hello
I am designing a boost converter and using UCC28C58 for control. The switching frequency of my converter is 40kHz and I need >50% maximum duty cycle operation. Can this IC provide switching signals at 40kHz…