Part Number: UCC29002 Hi,
My customer used the UCC29002 in parallel with two 1000W power supplies, and there has been a start-up issue.
Because the start-up time of the two sets of power supplies is different, it will cause the OPP condition. Is there any…
Part Number: UCC29002 Other Parts Discussed in Thread: UCC39002 Please clarify the differences btw the UCC29002D and the UCC29002D/1 bec E2E responses differ and the data sheet is a bit ambiguous. One e2e response says the difference btw the parts is…
Part Number: UCC29002 Hi Team
There is a good new that we DIN UCC29002
And there have one thing need your support! Please help check this SCH, THX
Cause need LS voltage is 8V, From the calculation formula below, I found out why R512 value cannot use 1…
Part Number: UCC29002 Hi team
My customer raised a new requirement and I am wondering if you could give a correct solution?
Supply#1: 12V, 1.25A max Iout
Supply#2: 12V, 1.25A max Iout
The customer wants to connect these two supply to one load and hence…
Part Number: UCC29002 Hi Support team
my customer encountered the unstable issue w/ UCC29002, we fingered out the way to mitigated the noise coupling from current shunt resistor after add 0.22uF between CS+ & CS-
my question here is to know any side…
Part Number: UCC29002 Other Parts Discussed in Thread: TPS2412 We are using the UCC29002 and TPS2412 in a load share / hot swap application. Looking into the forum this seems to be a common application.
Now I'm wondering how to deal with the LS pin maximum…
Part Number: UCC29002 Hello,
One of my customers, is using the UCC29002 load share controller. They have an application that uses this chip powered off of a 12V bias to load share for a 15V output, with the sense line essentially right on the adjust pin…
Part Number: UCC29002 Dear team
Is there any reference design for the application between the two PD chips of this UCC2900X Current Sharing IC?
Many thanks
Denny
Part Number: UCC29002 Other Parts Discussed in Thread: UCC28950
How are you ?
How to control the load sharing regarding the connection of the two parts.
Is there a circuit diagram for the UCC29002 and UCC28950?