Hi,
As we are in communication through email for the layout review, I will close this thread. If you have other support need, you can create a new thread.
Other Parts Discussed in Thread: UCC35706 Hi,
I am Trying to make one DC to Dc convertor with UCC35706, strangely all the four devices I had is gone bad ie PIN 3 Vff shows zero Volt.
The schmatic design is taken from another working design. Its resonant…
Hi Jeyaprakash
I do not see any PSPICE model for the UCC25706,UCC35705,UCC35706 devices either ?
Have tou found a model for these parts outside of TI?
Regards
Peter
Andreas,
TI general purpose, current mode PWM controllers can be set up for VMC by feeding the RAMP into the CS pin and they are not topology specific so they can be used for flyback, forward, buck, boost, etc. Configuring a CMC for VMC is a feature detailed…
Part Number: LM5021-Q1 Other Parts Discussed in Thread: LM5021 , UCC35706 , UCC35705 , UCC25706 , UCC25705 , UC3525A , UCC27517 Hi TI Team
I'd like to know the CS function of LM5021-Q1.
Could I disable this function?
I need a PWM IC could work on voltage…
Other Parts Discussed in Thread: UCC35706 , UCC25600 Input : 170 V AC to 265 V AC 50Hz
Output: 110V DC ,2A
Device Selection : ucc35706
With Flyback topology Input MOSFET becomes very HOT(Even with forced cooling),shall I go for Forward topology?