Part Number: UCC37322 Tool/software: hi sir
I am using this IC to drive the Pulse transformer and this pulse transformer drive the IGBTs SKM400gb12T4 connected in parallel. The NON SMD IC connected at the same circuit is able to drive the IGBTs whereas…
Part Number: UCC37322 Tool/software: I had ordered and got this IC https://www.ti.com/store/ti/en/p/product/?p=UCC37322DR
But there is not notch or markings to identify the pin orientation of the mosfet driver IC. how do I identify the pin no.s
Part Number: UCC37322 When VDD is 12V what is the recommended way to drive the Enable pin. Do I need a special driver. Can The ENBL pin pull-up be changed? Please provide some examples if available.
Im planning to use UCC37322 and implement this part…
Part Number: UCC37321 Other Parts Discussed in Thread: UCC5390 Dear TI experts,
I want to make 2x ucc37321 being in parallel that is connected directly to eachother pin for pin in order to enlarge the output current , Is that ok ?
Thanks,
John
Hi John,
Glad to hear from you!
Since you're using Vdd = 12V, the IN pin (#2) max is Vdd + 0.3 = 12.3V. Though your waveforms are looking good, it is generally best practice to give yourself some wiggle room and not operate the driver so close to…
Hi,
Has the request for the model for this UCC37322 been processed?
If not, what other gate driver already available on TINA-TI possibly comes close to this considering its a 9A driver.
Suggestions please.
Thanks
Abdul Nilar
Part Number: DRV110 Other Parts Discussed in Thread: UCC37322 I'm using the DRV110 in a design to drive a 120VDC solenoid in Peak and Hold operation.
When I increase the I_hold set point, the OUT gives me something that I don't expect: A long pulse…
Part Number: UCC37321 Other Parts Discussed in Thread: UCC37322 , around 2 or 3 months ago, I ordered 5 sets of ucc37321 and ucc37322, and around 1 week ago I got the time to use it in a project, but when I powered the project on, the ucc37321 ic keeps…
Hello Tim,
The parts could have originated from Unitrode. UCC27322DR also continued to be marked with the unitrode markings for some time after being acquired by TI. 1B is a two digit date code corresponding to year and month. Assuming B mean the second…