Part Number: UCC3800 Other Parts Discussed in Thread: UCC2801 , UCC2805 , UCC2804 , UCC2802 , UCC2800 Dear seniors,
I want to use UCC3800 to make a 2W flyback power supply.
Because the input voltage range is narrow, about 11.5V~12.5V, and the output voltage…
Other Parts Discussed in Thread: UCC3800 Hello,
I have a few questions concerning the overcurrent feature of the UCC3800:
Is it safe to pull CS up to 5V in order to shutdown the output? It seems like it is triggering the current limit comparator but not…
I would like to know if shorting Vref to ground will cause any damage or if there are any long term reliability concerns. I would like to use the Vref to shut down the PWM chip.
Thanks,
Michael Lin
Hello Jerry,
The attached application note describes the differences between the UCC3800 family and the UCC3813. The UCC3804 is a member of the UCC3800 family of controllers.
Regards,
Mike
UCC3800-3813 Differences slua247.pdf
Part Number: UCC3808-2 Hello everyone,
I am using the UCC3808 controller in a Push-Pull Topology. As the duty cycle at steady state would be greater than 50% it is almost imperative the use of slope compensation. The circuitry that I am using to achieve…
Hello Kaji@PAN,
Thank you for your interest in TI Parts. Other Low power BiCMOS: CMPWM that would fit these specifications are UCC2800/UCC1800/UCC3800.
I am attaching the link to a search on ti.com for similar parts, this list will be a good starting…
Other Parts Discussed in Thread: UCC3800 I want to design smps with input 8-30 V and output must be 12V 1.5 A 18W. Please suggest me the IC and please suggest me the reference design.
Other Parts Discussed in Thread: UCC2806 , UC1846 , UC2846 , UCC3800 I could not find a pspice model for UCC2806 on TI website. Does anybody know how to get it?