. UCC2805 with injected voltage spike in series with the resistor per pp. 5-6 of this app note …
U-133A UCC3800/1/2/3/4/5 BiCMOS Current Mode Control IC's Application Notes : http://www.ti.com/litv/pdf/slua149
Other Parts Discussed in Thread: UCC28950 , UCC3800 , UC2827-2 I'm looking to make a DC/DC conversion with:
an input range of 8V to 20V
output of 12V
and output current of 60A
Am I able to use a SEPIC to do this? If not, why not?
What…
Hi Steven, Thank you for your reply. Here's the Rev D slus270d.pdf Kindly see below the snippets.. Furthermore, I've checked the SLUS270F, it seems that the "line regulation" for the UCC380x is not copied on SLUS270G. Can you please help confirm? Thank…
Other Parts Discussed in Thread: TINA-TI Update of TINA9-TI Spice Model Libraries and Example Circuits
This note describes the step-by-step process for updating the TINA9-TI Spice Macro Libraries and Example circuits. The update is initiated by selecting…
Part Number: UC3844 Hi
I am Vasudev , I am designing 1.5kw 2 switch forward converter for which I am using UC3844 based current mode control to operate only in constant current mode at the output(of course with limited voltage range) . I am aware that…
Hello,
The UCC3806 is a dual output controller though it can be used in a flyback where only one of the outputs are used to drive the switch it might be better to choose a single output controller. Look at page 46 of the attached under General Purpose…
Siyu,
I think the toggle flip-flop in the block diagram on page one of the spec should have let you know that the max you will get with this device is 50% duty.
Go to page 43 and 44 of the attached and select a more suitable part.