Part Number: UCC3808-2 Other Parts Discussed in Thread: TL431 Hi
We have designed push pull converter using IC UCC3808-2. Input is 10 ~ 60V DC input from battery and output is 170V DC. Generated 170V DC is fed to inverter to get 110V AC output.
Please…
WEBENCH will work for SN6507 with VIN=9.8V, if you decrease the max VIN from the default 36V....reduce to something like VIN_max=30V, or whatever the max input voltage is for the design?
Yes, the output is unregulated so you have to either regulate the…
Part Number: UCC12040 Other Parts Discussed in Thread: UCC12050 , UCC33020 , UCC33420 , UCC15240-Q1 , UCC14140-Q1 , UCC14131-Q1 , UCC3808-2 Tool/software: Please recommend isolated DC/DC converters that is not a module power supply and has a withstand voltage…
Part Number: UCC3808-2 Hello everyone,
I am using the UCC3808 controller in a Push-Pull Topology. As the duty cycle at steady state would be greater than 50% it is almost imperative the use of slope compensation. The circuitry that I am using to achieve…
Part Number: UCC3808-2 Hello,
Hope you are doing well.
We designed PWM adjustable(0~40VDC) Push-Pull power supply by using UCC3808-2.We are facing below mentioned issue:
The final output voltage waveform looks as below :
So it should be stable DC voltage…
Part Number: UCC3808-2 Hello,
We are using UCC3808-2 for Generating 40V adjustable supply. Kindly find schematic in attachments.
We are providing Pulses as below :
1)"Dutycycle" = 100hz(10%,20%,50%,100%)
2)"PWR" = 100hz (0.1us increment)…
Part Number: UCC3808-1 Other Parts Discussed in Thread: UCC3808-2 Hi We need to design push pull converter with following specification.
Vin: 10V to 60V DC
Vout: 160V DC
Iout: 1.3A
Wattage: 200W
Efficiency: >90% at full load; >80% at 60W laod
I exported…
Part Number: UCC2808A-1 Other Parts Discussed in Thread: UCC3808-1 , TL431 Hello,
I would appreciate if somebody could help me fixing a problem affecting an old design initially based on an UCC3808-1 and now using an UCC2808A-1.
Regards
Gilles
We are using…