Part Number: UCC38083 Other Parts Discussed in Thread: UCC3808A-1 I am currently trying to Design a feedback control loop for a switching power supply design using the UCC38083 and the UCC3808A-1. I am trying to bread board them before laying out a PCB…
Hi,
50 W Push Pull Converter reference design using the UCC38083 (Rev. A) (ti.com)
How to prevent transformer saturation in push-pull converters
LM5030 Application: DC - DC Converter Utilizing the Push-Pull Topology
1.5_Mhz_Current_Mode_IC_Controlled_50…
Part Number: UCC38083 Looking at the reference design on this part's datasheet (Fig 5, p 11), is there a design procedure for C9, R13 / C14, R17, and similarly for C16 and R20? Any help would be greatly appreciated.
Thanks in advance,
Brian
Part Number: UCC38083 Hello, I'd like to ask for advice about UCC38083.
How could I disable the function that cycle-by-cycle current limiting causes the PWM stop and then soft-start .
I'd like to only employ the function of cycle-by-cycle current…
Part Number: UCC38083 Other Parts Discussed in Thread: UCC28083 Team,
Can you please confirm the below: -The datasheeet gives the min/max " start threshold voltage " page 3 of SLUS488E . Can it be assume that the VDD min/max specs are the same as…
Part Number: UCC38083 Hello, I am an engineer and working for Ablerex. I am interesting to use a PWM IC, UCC38083, and employ it to implement a DC/DC full bridge converter. However, I can't do well on the compensation for it, which causes the output inductor…
Hi,
We do not have a design on your specs. For push-pull similar reference designs:
50 W Push Pull Converter reference design using the UCC38083 (Rev. A) (ti.com)
LM5030 Application: DC - DC Converter Utilizing the Push-Pull Topology
There are more on…
Part Number: UCC38083 I am interesting to use a PWM IC, UCC38083 , and employ it to implement a DC/DC full bridge converter.
Unfortunately, the pulse current of MOSFET is very large as the output short- circuit test,
because I must choose a smaller current sense…
Hello BJE,
I searched through TI's Reference Design Library , but did not find anything close.
I then used Webench with the following specifications: 40-65Vin, 500Vout, 1Aout (500W), isolated output. Then chose a low cost solution with internal soft…
Other Parts Discussed in Thread: UCC38083 Spec : 1.Vin=42V
2.Vo= 24V
3.500W DC-DC Converter
Can you provide two solutions? THX
1. DC-DC Converter + GAN +SR
2. DC-DC Converter + MOS +SR