Part Number: UCC3809-1 Tool/software: Dear Team,
Currently I am designing flyback converter. There while selecting input electrolyte capacitor do I need take care about ripple current at input side ? if yes what is the best way to calculate this input…
Part Number: UCC3809-1
Here at our company we have a product that includes a UCC3809DTR-1 SOIC-8 chip in a flyback topology (schematic included). This product is running in the field for quite some time (10+ years) but suddenly we're experiencing a…
Part Number: UCC3809-1 Hi,
May I know is there any equivalent component of UCC3809 with automotive grade?
Thanks in advance.
Best regards
Shwetha Ramachandra
Part Number: UCC3809-1 Hi Team,
My customer is looking for the Unencrypted SPICE model of our UCC3809-1 to be used in a third party simulator tool.
Can you share the Unencrypted SPICE model of our UCC3809-1?
Regards,
-Renan
Part Number: UCC3809-1 Other Parts Discussed in Thread: TINA-TI Hello,
I would like to simulate the 10 Watt circuit found in the application note SLUU087B (attached below) using the UCC3809-1 controller in the TINA-TI simulation software.
http:…
Part Number: UCC3809-1 Hi there,
I am learning TI slua086 , p7-8 talks about three parameters to consider on diode selection in flyback. I have some questions to consult.
(1) Quote page8 "The peak repetitive forward current is equal to the reflected…
Other Parts Discussed in Thread: UCC3809-1 , TPS40210 Hello,
I'd like to design a flyback isolated DC DC Converter with the following specification :
Vin = 10V to 30V
Vout = 48V
Iout = 1.5A (max)
With such power 72W, the first choice is…
Hi, sorry I missed this one can you share a block diagram showing what you are trying to do? We also have PMP8906 which is another example of how to use the UCC39002.
Is this closer to what you are looking for?
PMP8906 REVB SCH 02-28-2013.pdf…
Other Parts Discussed in Thread: UCC2809-1 , PMP Are any EVMs or PMP's offered for the UCC2809-1 (or 3809)? I can't find an EVM, and there is a big list of PMP's here http://www.ti.com/product/ucc3809#toolssoftware but I don't know if any are availabile…
Hi John,
i have been able to attach the files.
Best regards,
Stefan
56V_0.35A flyback Mathcad pdf.pdf
Power Tip #98 - Designing a DCM flyback converter.pdf
PowerTips Designing a CCM flyback converter.pdf