Part Number: UCC3895 Hello,tech support
could you help to check the die marking on below picture
why this part didn't have the TI logo?
thanks and looking for your reply.
B.R.
YINGCHUN
Hello, I learned from the data sheet of ucc3895 that ucc3895 can work in current mode or voltage mode. In current mode, the RAMP pin is connected to the CS pin. And in voltage mode, The RAMP pin is connected to the signal at CT. I want ucc3895 to work in voltage…
Hello,
I reviewed your schematic and waveforms.
I reviewed your schematic and the design seems to be setup for some kind of half bridge and not a full bridge. The UCC3895 is not designed for this configuration. This is most likely what is causing your…
Part Number: UCC3895 Other Parts Discussed in Thread: UCC2895 , UCC28950 , UCD3138 Dear Sir or Madam, I am currently using UCC3895 for Peak Current Mode control PSFB PWM generator.
I read the datasheet and I set the current sensor value of 0-2V, the frequency…
Part Number: UCC3895 Other Parts Discussed in Thread: PMP9622 , UCC28950 Hi Team,
i have designed a power supply using UCC3895 and its working fine without feedback but as soon as i connect the feedback circuit to the IC it doesn't work, So i am attaching…
Part Number: UCC3895 Other Parts Discussed in Thread: UCC39002 , UCC29002 , UCC2895 Hi team , 1- Can we adjust the output voltage by change the uC duty cycle Like this figure below? the uC generates PWM signals and the signals are filtered ( converted ) to…
Part Number: UCC3895 Other Parts Discussed in Thread: UCC28951 , UCC28950 , UCD3028 , TSC2000 Dear Team,
I need a voltage output which should vary from +Out to -Out. I use a phase shifted transformer driver, as you use in the App Note SLUA287 – March 2003…
Part Number: UCC3895 Other Parts Discussed in Thread: UCC2895 Hi,
I read the SLUA501 application note "UCC2895 Layout and Grounding Recommendations". Can I put the "quite ground plane" and "power grpund plane" in the same PCB layer or I have to put them…
Part Number: UCC3895 Other Parts Discussed in Thread: UCC2895 , UCC256402 , UCC28951 , UCC28950 I use the 3895 chip as the main control chip of the LLC resonant converter, which adopts single voltage control. At the same time I wanted to use the CS pin for…
Part Number: UCC3895 Other Parts Discussed in Thread: UCC28950 We are designing DC to DC converter using UCC3895 . Input is 24VDC and Output is 12VDC (5A current). We need to know that is Current transformer at the primary side is required for our design…