Part Number: UCC3895 Other Parts Discussed in Thread: UCC28950 We are designing DC to DC converter using UCC3895 . Input is 24VDC and Output is 12VDC (5A current). We need to know that is Current transformer at the primary side is required for our design…
Part Number: UCC3895 Other Parts Discussed in Thread: UCC28951 , , UCC2895
I am designing a 3KW CC/CV (60V 50AMP max) power supply and I choose UCC28951 PSFB controller but this part is out of stock and I can't get it so my question is can I design a…
Part Number: UCC28070 Other Parts Discussed in Thread: UCC28950 , UC3854 , UCC3895 , 想設計一個交換式電源供應器 , 三組輸出電壓總功率約2.5kw
想請問有UCC3895 or UCC28950 相關參考設計嗎? 並搭配 UC3854 or UCC28950 BOOST PFC 電路
Part Number: UCC3895 Other Parts Discussed in Thread: UCC28951 , , UCC2895 , UCC28950 , Greetings,
At least one section in this datasheet seems to have been lifted directly from the datasheet for the UCC28951 and does not apply to the UCC3895.
Specifically…
Part Number: UCC3895 Other Parts Discussed in Thread: UCC28951
Hi team,
UCC3895 is a non support SR control solution, so many user choose OUTA and OUTB signal for SR control.
But still has some project choose OUTB and OUTD for SR control.
What is the…
Part Number: UCC3895 Other Parts Discussed in Thread: UC1875-SP OK, I understand; I'm straight now.
I'm only using the UCC3895 as it comes with a SPICE MODEL and it's a close cousin to the UC1875-SP, that has "NO" SPICE MODEL. I will eventually need…
Part Number: UCC3895 Other Parts Discussed in Thread: UCC27200 This is an add question from a previous request concerning the UCC3895 drive specification. I trying to understand the DRIVE capabilities of the OUT-A,B,C,D. I am reviewing the data sheet…
Part Number: UCC3895 I am designing a PSFB using the UCC3895. I'm looking at SLUS157Q, page 8 of the data sheet "OUTPUTS". I see High Output = 250mv TYP, and Low output = 150mv Type.
These parameters are stated for ALL OUTPUT. I don't think…
Part Number: UCC3895
Hi team,
When we use external clock for UCC3895 to SYNC-pin, what do we need to do to CT and RT-pins
Can we just leave float these pins? or do we need to connect to somewhere?
If you have any example schematics, could you please…
Part Number: UCC3895 Other Parts Discussed in Thread: , UCC28951 , UC1875-SP I am designing a Phase Shift Full Bridge Power supply. I will be using the UCC3895 device. I am also taking some tips from one of the TI Eval boards using the UCC3895. The board…