Part Number: UCC5350 Other Parts Discussed in Thread: UCC5320 , UCC5390 Dear HPD Experts,
The ucc5350m has a UVLO of 12V while the ucc5350s has a UVLO of only 8V.
Any reasoning behind this?
Especially as ucc5320 and ucc5390 has the same UVLO irrespective…
Part Number: UCC5350 Hi Expert,
In my customer's application, the trace between the controller output and UCC5350 input is long, to improve the performance against noise, the solutions come in my mind include:
1. RC filter before UCC5350 input;
2…
Part Number: UCC5350-Q1 Other Parts Discussed in Thread: TINA-TI Hello,
I am using this to drive a SiC mosfet and the simulation is being done on TINA-TI, but I am not getting anything at the output that looks like a pulse.
Note: This is PWM_LO_1
I…
Part Number: UCC5350 Hi team,
Below is the schematics to drive Infineon SiC CoolMOS, which VEE2=0V is enough for switching off. Is there need any protection circuit such as TVS clamp here?
Thanks.
Part Number: UCC5350-Q1 Hi Team,
My customer Preh has a question about the UCC5350-Q1:
How to calculate the RMS current for gate drivers. 4x Gate Driver UCC5530 for H-bridge control are in use and a Gate Driver will each drive an IGBT, which each IGBT…
Part Number: UCC5350 Hello Support team,
My customer ask NMOS and PMOS ON timing between VCC2 and OUT, is the on timing of NMOS and PMOS same?
Thanks,
Koji Ikeda
Part Number: UCC5350-Q1
When does TI get safety-related certifications for DWV package of VDE and UL?
I see it is still “Certification planned” at the data sheet.
Part Number: UCC5350 Hello expert,
Our customer is asking if this part#ID on the die is that of part# UCC5350SBDR
Appreciate your expert advice.
Thank you.
/resized-image/__size/320x240/__key/communityserver-discussions-components-files/196/UCC5350SBDR…
Part Number: UCC5350 Dear Expert ,
Good day!
Our customer use UCC5350MC as the gate driver , here is schematic:
,
Now , the Mosfet without load , Pin1 do not have power , the customer test the signal wave between pin 3 and pin 4
1 . R16 change to 2Ω ,…
Part Number: UCC5350-Q1 Hi team,
How much VCC2 Negative-going UVLO threshold voltage is?
I just found datasheet says its minimum and typical value as 10.3V and 11V respectively, how about its maximum?
Regards, Ochi