Part Number: UCC5350-Q1 Other Parts Discussed in Thread: TINA-TI Hello,
I am using this to drive a SiC mosfet and the simulation is being done on TINA-TI, but I am not getting anything at the output that looks like a pulse.
Note: This is PWM_LO_1
I…
Part Number: UCC5350-Q1 Hi Team,
My customer Preh has a question about the UCC5350-Q1:
How to calculate the RMS current for gate drivers. 4x Gate Driver UCC5530 for H-bridge control are in use and a Gate Driver will each drive an IGBT, which each IGBT…
Part Number: UCC5350-Q1
When does TI get safety-related certifications for DWV package of VDE and UL?
I see it is still “Certification planned” at the data sheet.
Part Number: UCC5350-Q1 Hi team,
How much VCC2 Negative-going UVLO threshold voltage is?
I just found datasheet says its minimum and typical value as 10.3V and 11V respectively, how about its maximum?
Regards, Ochi
Part Number: UCC5350-Q1 Dear. TI engineers
VCC2 is using 15V and VEE2 is -5V.
1. Should the clamp pin be connected to the FET's GATE? or do I need to connect to VEE2?
2. And what's the difference when connected to GATE or VEE2?
Best regards…
Part Number: UCC5350-Q1 Hello,
my customer is currently working on a design and uses UCC5350-Q1 with integrated Miller Clamp a s an IGBT driver.
They would like to get more information about the Miller Clamp feature and are particularly interested in:
…
Part Number: UCC5350-Q1 Other Parts Discussed in Thread: UCC21320-Q1 Hi team,
Is "IN-" pin used such as "DISABLE" input pin? Table 4. Function Table looks IN-=DISABLE(driver output=L with high level input), which is the same function…
Part Number: UCC5350-Q1 Hello team,
My customer wants to know input capacitance of IN+/-pins What is the typical capacitance of the input pin? That information is requested to check the source / sink current of the MCU's I/O port driving the IN +/- pins…
Part Number: UCC5350-Q1 Hi Team,
The datasheet of UCC5350-Q1 states the part-to-part skew of the propagation delay is given as 1ns typical and 25ns maximum. For a planned application of the customer this specific characteristic is very important and 1ns…