Part Number: UCC5390 I am doing a Gate Drive Signal Test.
I am using UCC5390SCDR to drive 3 FF07007M2K in parallel with 100khz 3.3V pwm driving voltage 16-0V and 0 Rg 0 Vds.
The MOS total amount Qg is 975n.
I used the formula in Ti datasheet page…
Part Number: UCC5390-Q1 Other Parts Discussed in Thread: UCC5390 Tool/software: Hello,
While reviewing reference designs for the UCC5390-Q1 isolated gate driver, I found a circuit similar to the attached schematic. In this design, Schottky diodes are…
Part Number: UCC5390 Dear Team,
We are using the C3M0016120K Wolfspeed MOSFET in our inverter design and would appreciate your recommendation for a suitable gate driver.
The required specifications are as follows:
MOSFET: C3M0016120K
Source…
Part Number: UCC5390 Hello Experts,
In UCC5390 Single-Channel IsolatedGate Drivers i have facing some issue as we apply ouput voltage of +15V and -5V but the ouput i am getting is +15V and -3.4V why that negative voltage drop is occuring i dont get…
Part Number: UCC5390 Hello E2E Experts,
VCC2 and VEE2 pins of the spice model of UCC5390ECD gate driver draws 4A when the gate is off.
It does not happen with the actual device.
Regards,
TICSC
Part Number: UCC5390 Tool/software: When I use UCC5390SCDR to drive MOS, VCC1 pin is powered by 5V, IN- pin is directly connected to GND1 pin, VCC2 pin is powered by 15V, and VEE2 is 0V,and my controller is stm32G474 seires and I can detect the 3.3Vpwm…
Part Number: UCC5390 Other Parts Discussed in Thread: UCC5350 , TVS0500 Tool/software: Hi,
I'm using the UCC5390SC in a single-phase UPS application. One of the six gate drives used in the device is sometimes damaged during startup.
When the UCC5390SC…
Part Number: UCC5390-Q1 Other Parts Discussed in Thread: UCC5350-Q1 Hi Team,
I am looking for pratical test data information for Pulse rise time (tr) & Pulse fall time (tf) with Miller clamp option. As it was mentioned in datasheet w.r.t Capacitive…
Part Number: UCC5390 Other Parts Discussed in Thread: UCC5350 , UCC5310 , Tool/software:
I hope you are doing well.
I have designed an FET drive circuit using the UCC5390S, but I am currently experiencing significant FET ringing and am seeking a…