Part Number: UCC5390ECDWVEVM Other Parts Discussed in Thread: UCC5390 Tool/software: Hi team,
Our EVM only showed wrong pin out of UCC5390 on the output. Can you help provide reference schematic and layout when driving two parallel SIC FET by using…
Part Number: UCC5390-Q1 Other Parts Discussed in Thread: UCC21750-Q1 ,
Hi Team,
UCC21750-Q1 features the PWM interlock for IN+ and IN– pins, which can be used to prevent the phase leg shoot through issue.
But customer want to use UCC5390-Q1 is upper…
Part Number: UCC5390 Hi,
I am studying on isolated and non-isolated gate drivers for IGBT driven motor drive applications. My application area is three-phase two-level motor drives. I can understand that using all 6 switches with isolated gate drivers…
Part Number: UCC5390
Hello! I made a custom evaluation board to make some tests of UCC53xx drivers for my applications. Below you can see the first variant of the board with UCC5320C (Ron = 10 Ω , Roff = 5 Ω, VCC2 = 16V, VCC1 = 3.3V). In the first test…
Part Number: UCC5390 Other Parts Discussed in Thread: TINA-TI Dear TI team,
I am using IC UCC5390ECDWVR for gate driver circuit design. I am trying to simulate this circuit in TINA but I am getting errors and not able to resolve it.
Kindly suggest…
Part Number: UCC5390 Hi Team,
My customer is considering UCC5390S.
From following, RNMOS||ROH for UCC5390S is around 0.71Ω.
Is it correct the gate resistance should be chose from "gate resistance recommended by IGBT datasheet" -0.71Ω?
Thanks…
UCC5390E, Driver side Power Supply problem
I am using DC5390E, have dual power supply +15, -3 V, wRG, when I connect it to the chip it drops to +5 and .-0.33 volt. WRTG? Caps between GRND and VCC2 and VEE2 are connected.as per data sheet.
Part Number: UCC5390
Hello,
We are developing a full bridge three phase active recitifier where we implemented your UCC5390E gate driver. The rectifier is designed in a way that the driver circuits are located on separate PCBs (one PCB per driver…