Part Number: UCC5390-Q1 Other Parts Discussed in Thread: UCC5390 Tool/software: Hello,
While reviewing reference designs for the UCC5390-Q1 isolated gate driver, I found a circuit similar to the attached schematic. In this design, Schottky diodes are…
Part Number: UCC5390-Q1 Hello,
We are using the IGBT transistor IKW40T120 as a low-side switch with a 8 pulse train of 5KHz (D=0.5) with VGE=15V. The power supply is 800V and we expect to use this equipment with instantaneous 30A current. Each train…
Part Number: UCC5390-Q1 Other Parts Discussed in Thread: PSPICE-FOR-TI Tool/software: Hello, I am looking for an IBIS Model for Part Number "UCC5390ECQDWVRQ1", appreciate any help!
Part Number: UCC5390-Q1 Other Parts Discussed in Thread: UCC5390 , UCC23525 , UCC23711 , UCC21750 , UCC5350 Tool/software: Hi TI
I am currently working on a SST project in this we using the SiC MOSFET from microchip( MSC025SMA330B4N) having the rating…
Part Number: UCC5390-Q1 Other Parts Discussed in Thread: UCC21750-Q1 ,
Hi Team,
UCC21750-Q1 features the PWM interlock for IN+ and IN– pins, which can be used to prevent the phase leg shoot through issue.
But customer want to use UCC5390-Q1 is upper…
Part Number: UCC5390-Q1 Curves in the datasheet are mostly for 3.3V or 5V VCC1. As a critical component, are there any considerations, tradeoffs to using 12V? Will propagation delay be affected?
Thanks
William,
**Could you clarify whether you are working with the physical EVM or Webench design ?**
If you are simulating the EVM design using the PSPICE model from the UCC5390-Q1 project folder , theres no special configuration that needs to be done…
Part Number: UCC5390-Q1 Dear all
I designed a driver board with UCC5390-Q1 and noticed that the temperature rise on the IC was higher than my expectation.
Below is the circuit schematic. The PCB layout basically follows the recommendation.
Testing…
Part Number: UCC5390-Q1
Hello,
Could you please details the behavior of the OOK modulation ?
What is the TX carrier frequency of the UCC5350MC isolator stage?
Thanks,
Part Number: UCC5320 Other Parts Discussed in Thread: UCC5390-Q1 , UCC5390 ,
Team,
-Assuming that customer is using UCC5320ECD in an existing design:
-Can it be replaced directly by UCC5390-Q1/UCC5390? UCC5390-Q1 vs UCC5390 vs UCC5320 or are some…