Part Number: UCC5871-Q1 Hi Expert,
My customer is using UCC5871-Q1 in their project. When they change the RGON and RGOFF to 200Ohm, the OUTH voltage goes into 13V rather than normal 18V.
From my perspective the 2 resistors are used to minimize ringing…
Part Number: UCC5871-Q1 Hi Expert,
My customer is using the latest silicon in their project, only to find that the VCC1 UVLO is triggered. However, the voltage of VCC1 is 5.12V which is higher than level2. What's more, when customer disable VCC1 UVLO…
Part Number: UCC5871-Q1 Hi Team,
I'm looking for SPICE model of UCC5871Q Gate driver for one of my power supply designs. While checking on TI website, it was mentioned as request (i raised a request but didn't get any response).
It would be helpful…
Part Number: UCC5871-Q1 Hi experts:
For the application of ucc5871-Q1, we have some issue. As the picture showed below, When the short circuit happens, we will open the SIC-MOSFET, there will be a high voltage at Vds of MOSFET because of parasitic loop…
Part Number: UCC5871-Q1 Hi Expert,
For the application of ucc5871-Q1, we have some issue. As the picture showed below, When the short circuit happens, we will open the SIC-MOSFET, there will be a high voltage at Vds of MOSFET because of parasitic loop…
Part Number: UCC5871-Q1 If we drive the SiCMOSFET with 18V and -5V from ucc5871, can the Miller clamp protection function active?
And from the pic above, What is the ground for ISTO, is it VEE2?
Part Number: UCC5871-Q1 hi expert
i find the following picture from datasheet about DESAT function.
i have a question about tleb. from my understanding, the begin of tleb is rise edge of OUTH as quick calculation tool shown(tdesatleb), am i right?
do…
Part Number: UCC5871-Q1 Hi team.
My customer plans to use UCC5871-Q1 to driver SiC MOS instead of pyrofuse for faster react time, and in their configuration there's only one FET. I'd like to check with you:
If not bridge configuration, customer…
Part Number: UCC5871-Q1 Hi Experts,
We would like to know the minimum and maximum R(ON) resistance of the gate driver IC.
Seems the information is not available from datasheet.
Regards, Archie A.