Part Number: UCC21710 Other Parts Discussed in Thread: UCC5880-Q1 , UCC5871-Q1 , UCC5390-Q1 Hello everyone
We want to use UCC21710 to drive two SiC Mosfets in parallel. We need a peak current up to ±15A for two Mosfets total with rise and fall times <50ns…
Part Number: BQ79731-Q1 Hi Expert,
I want to confirm with you about the MSPI mode in BQ79371-q1.
You can see the structure shown below.
DSP communicate with 79600 via spi
79600 and two 79731 form a daisy chain string
Device1(79731) communicate with…
Hello Jay,
Thanks for reaching out on E2E.
Jay wang said: Q1: if we use 3860V DC to test UCC5870, it will damage UCC5870. is it right?
The RMS voltage of a DC voltage is equal to the DC value, so testing for 3750V DC for 1 minute will not damage the UCC5870…
In the spreadsheet, for IQ_DRIVER_VDD & IQ_DRIVER_VEE should I include the max load currents of 80mA & 10mA (i.e. UCC14240 EVM specs) or just the device's quiescent current?
[ANS]: IQ_DRIVER_VDD(VEE) is the gate driver quiescent current but you…
Part Number: UCC5870-Q1 Other Parts Discussed in Thread: UCC21750 , ISO5851 , UCC21710 , UCC21540 Hello everyone,
I am building a grid connected system, which consists of a three phase inverter (2 level AFE) and two parallel DC-DC converter (LC-SRC) which…