Hello BatMan,
You are right that the output would be almost zero at that point. This is limited by the size of the EADC since it is only 6 bits (max of 63). Thus, you cannot have Kp = 1 since the DERR is too small. Kp must be in the hundreds, if not…
I try to short 1.2V output to ground during power up sequence. After power up, remove the short but 1.2V always no power output. But other power rails all turn on. In this situation, 1.2V EN drive by UCD asserted but UCD GUI only show 1.2V power good…
I am trying to determine why I cannot program the UCD3138 easily through the FT4232HL IC, despite my timing being similar to the dongle's timing. The FT4232HL itself seems to be functioning properly; when I disconnect it from the UCD3138 eval kit (UCD31380L40EVM…
Manos Giatrakis said: I have tried replicating the results of Hardware Trace Analyzer with the function call sequence graph etc. in the latest version of CCS Theia and the only thing I can see being available is the Core Trace/Discontinuity trace.
That…
Hello Eduardo,
The PMP20873 is a good design that will work with your requirements. You will need to make hardware changes (mainly the boost inductor) to increase the power to 1kW. The code should work as is with the new power level.
The UCD3138 comes…
Part Number: UCD90320 Hello expert,
My customer is using UCD90320 in their switch project and would like to know if they can use GPI to set an interrupt to restart specific power rail. I found out GPI fault response might be suitable for this case.…
Thanks for the reply, Ishtiaque! We have UCD9090 in the same system that does the sequencing and also monitors the voltages and logs the faults. Looking at the UCD logs, it shows that it saw the UV fault for buck3 first as the main cause of this fault…
Hi,
Unfortunately the third party that developed the DCA1000 is no longer available for support.
All the documentation available is included in the mmwave studio package
C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\ReferenceCode\DCA1000
Some…
Part Number: UCD9090A Tool/software: Hi team,
There is a document that mentioned how to loading the configuration from CPU to device.
1007.Configuration Programming of UCD Devices (2).pdf
Do we have any example code for customer to demo the coding…