Hi Michel,
CVCO55 series footprint fits the eval board.
Frequency range and phase noise of the VCO are the key parameters that must suit your application need.
Other key parameters, such as tuning sensitivity and input capacitance are used for the loop…
Stone
Thanks for your post. Looks like the output is unstable. If you are extremely unstable, a DVM would measure half supply (1.65V) at the output since the output is constantly toggling between 3.3V and 0V. Please checkout our TI Precision Labs training…
Hi Liang,
Zhang Liang said: they consider to use the Line out 5V RMS@ 100ohm, the load power is about 500mW;
https://www.ti.com/amplifier-circuit/op-amps/audio/products.html#1typ=2%3B13&sort=451typ;desc&
OPA1621 and OPA1622 may meet the power dissipation…
Hi Kyle,
Thanks for reaching out about our CAN transceivers!
If you are looking for information on the CAN standard, I would highly recommend our Precision Labs video series which goes into on this. It is an excellent training resource with helpful visuals…
Hi A Yang,
Please see the training lab video on the UCD locked flash problem: https://www.ti.com/video/series/introduction-to-digital-power-controllers.html . Specifically, "UCD3138 Digital Power Tools: Boot ROM and program flash checksums" at the 4:00…
Part Number: PMP23340UCD Other Parts Discussed in Thread: UCD3138A , UCD3138 HI guys,I encountered a problem when configuring the compilation environment.
Environment:Code Composer Studio 12.5.0(Compiler version [TI V5.2.9])
Part number:PMP23340UCD …
Rasty,
The examples are applicable for AM57.. as seen in the link I sent:
Josue Zamitiz-Ayala said: The Training for PRU is here: https://software-dl.ti.com/processor-sdk-linux/esd/AM64X/08_06_00_42/exports/docs/common/PRU-ICSS/Overview.html#:~:text=PRU…
Hi Emin,
I do not think you need to worry about looking into the code of the .x0 file. Can you confirm that you have followed the Getting Started steps as explained in this E2E post: https://e2e.ti.com/support/tools/code-composer-studio-group/ccs/f/code…
Part Number: TMS320F280039C Other Parts Discussed in Thread: LAUNCHXL-F280039C , BOOSTXL-BUCKCONV , SYSCONFIG , POWERSUITE Tool/software: Hi,
I am providing a training on digital control for power electronics next week, using LAUNCHXL-F280039C and BOOSTXL…
Hello Kaveh,
Thank you for your interest in UCD3138x devices . The UCD3138x devices should work in your application. In the block diagram, all of the grey lines show possible connections between blocks. While normally designers set the DPWM based on a…