Part Number: UCD3138064 Other Parts Discussed in Thread: UCD3138 Hi TI experts,
Can you provide sample code with UCD3138064 manually acknowledge to PMBUS slave address?
Thanks!
Part Number: UCD3138064A Other Parts Discussed in Thread: UCD3138064 , Hello, I'm trying to migrate existing code from UCD3138064 to UCD3138064A. We are using the SPI bus with CS on pin 35 (FAULT0), SCLK on pin 36 (FAULT1), MOSI on pin 38 (TDO) and MISO…
Part Number: UCD3138064 Other Parts Discussed in Thread: UCD3138 Hi TI experts,
When UCD3138064 PMBUS Address is set 0x58 and SLAVE_MASK=0x7F, I try send 0x7F address but it return ACK.
I want to implement send I2C address 0x7F return NACK, how…
Part Number: UCD3138064 Other Parts Discussed in Thread: UCD3138128 Tool/software: Dear,
I got a problem on UCD3138064 when I used the FusionX0ToHext to convert the X0 file .
I solved the UCD3138128 via the FusionX0ToHext to convert the X0 file…
Part Number: UCD3138064 Other Parts Discussed in Thread: LM51770-Q1 , UCD3138 , PMP23377 Hi team,
Can LM51770-Q1 support 1000+W output with 12V/140A? Do we have any reference design or materials for this application?
Regards,
Eileen
Part Number: UCD3138064 Other Parts Discussed in Thread: UCD3138 , , USB-TO-GPIO2 I used ucd3138 as the main control chip for the bridgeless totem-pole PFC power supply. After manually running the code using the Device GUI, the bridgeless totem-pole PFC…
Part Number: UCD3138064 Other Parts Discussed in Thread: FUSION-PRODUCTION-GUI Tool/software: Dear Sirs,
Regarding the pflash checksum configuration issue in FUSION-PRODUCTION-GUI: When setting up the pflash checksum option in the programming interface…
Part Number: UCD3138064 Other Parts Discussed in Thread: UCD3138 , UCD3138128 Tool/software: Dear Sirs,
I have a question to ask: Due to CRPS2.0 requirements, I need to develop a bootloader. Currently, the firmware download and Flash write operations…
Part Number: UCD3138064 Tool/software: I have two questions about the CCS environment.
1. How do I choose the Output format for my new project? What is the difference between the them?
2. When choosing eabi it can be compiled, but there is no .x0…
Part Number: UCD3138 Tool/software: I need for "checksum" code conversion from UCD3138064 to UCD3138128. May I ask if there are any relevant documents that I can refer to?