Part Number: UCD3138064 hi, I want to have one program flash of 64 kB in UCD3138064x (no dual images and switching between two images, one simple 64 kB image)
I did start to work on Lab examples and the linker file cyclone_64.cmd is configured only for…
Part Number: UCD3138064
hi, my program uses all 64KB for code. I would like to enable MFBALRx read only protection for both flash banks
flash bank 0 was easy: add TI example code to the asm loader LDR r4,c_mfbalr1_half0 ;point r4 at program flash base address…
Part Number: UCD3138064 We are referring your document for pull up resistor calculation ( /cfs-file/__key/communityserver-discussions-components-files/196/I2C-Bus-Pullup-Resistor-Calculation.pdf ) for UCD3138064RJAR controller. We are not able to find out…
Part Number: UCD3138064 Hi all,
I am asking for my customer.
Since the I2C specification defines 10kHz of minimum I2C speed, but I check the UCD3138064 datasheet does not specify about it (pic below).
May I confirm does the UCD3138064 device support…
Part Number: UCD3138064 Hi team,
I have a confusing question about the PMBUS connection.
There are two kinds of resistor value in series with PMBUS_CLK and PMBUS_DATA
(1)33.2ohm
(2)100ohm
if there is a design guideline for these resistors? the value…
Part Number: UCD3138064
Hi Champ,
I am asking for my customer.
Currently, the customer attempts to use PCM slope compensation (FeCtrl2Regs.DACSTEP.bit.DAC_STEP) to limit the duty.
Is it feasible to use the parameters( DAC_STEP ) to calculate how much the…
Part Number: UCD3138064 Hi,
I'm working on a custom 2kB bootloader for the UCD3138064.
Where can I find some example code of a 2kB boot flash program on the UCD3138064? Preferably using UART as the communication interface as a command interface for…
Part Number: UCD3138064 Other Parts Discussed in Thread: UCD3138 Hi experts,
- I would like to use DCOMP for fast interrupt when FE0 exceeds a particular value, and I found when I try to enable the IRQ and FIQ, UCD3138 will be brick. (Can not search for…
Part Number: UCD3138064 Hi Champ,
I am helping my customer out the current limit module currently.
How much delay time will the detection be, when the current limit module of DPWM triggers ?
May I make sure is it 70ns written in the datasheet ?
Thanks…