Part Number: UCD3138A Hardware: UCD3138A, XDS100v2 Software: CCS 12.8, TI ARM CGT 20.2.7.LTS
I would like to share some experimental findings regarding JTAG lockout on the UCD3138A.
After programming a valid Flash checksum at 0x7FFC , the device boots…
Part Number: UCD3138A Other Parts Discussed in Thread: UCD3138 Tool/software: Hello:
The application issues for customer UCD3138A are as follows: The application is a constant current source project, and during debugging, it was found that there…
Part Number: UCD3138A Dear Team,
I am planning to use the UCD3138A for an active-clamp phase-shifted full-bridge (PSFB) zero-voltage transition (ZVT) topology. Is it feasible to implement this control logic using the UCD3138A?
Part Number: UCD3138A Other Parts Discussed in Thread: USB-TO-GPIO2 , , FUSION-DIGITAL-POWER-STUDIO Hi champs,
I am asking for our customer.
The user wants to use UCD3138A and USB-TO-GPIO2 for design/program.
The user wants to check if TI has…
Part Number: UCD3138AUCD3138A team,
Can you explain how the I2C address is defined based on R-ADDSET? It is mentioned in figure 7-13 of the datasheet, but I don't see any further specifics in the datasheet or User Guide.
Thanks, Darren
Part Number: UCD3138A Other Parts Discussed in Thread: UCD3138 Hi,
I have received a few questions regarding the UCD3138A that I need some help with:
1) Is there any info on what kind of driver/receiver is being used for the SDL and SDA nets?
2…
Part Number: UCD3138A Other Parts Discussed in Thread: UCD3138 Tool/software:
Hello,
I'm trying to get started with the UCD3138, following the video and after importing the Lab 1 project, on properties I don't find the same functions as on the video…
Part Number: UCD3138A
Tool/software:
Hi Team,
1. We want to check that is it possible to implement the hysteretic current control using 3138A? If so, can you share any model/example or which modules to use?
2. For AC signals control, like sinusoidal…
Part Number: UCD3138A Other Parts Discussed in Thread: UCD3138128 , UCD3138 Tool/software: Hi,
The CIM on UCD3138A does not have the mask for UART0, only UART1 and 2
Is the UART0 using a different interrupt handler? And how do I figure it? It will…
Part Number: UCD3138A Other Parts Discussed in Thread: UCD3138 , USB-TO-GPIO2 Tool/software: Dear TI Support Team,
I am using the UCD3138A along with CCS version 12.8.0.00012 to generate the .x0 file.
Additional details:
Fusion Digital Power Studio…