Part Number: UCD3138PSFBEVM-027 Other Parts Discussed in Thread: UCD3138 Hello everyone hope you re good !
I want to know how can i get measurement of the EADC input (EAP0) using the UCD3138 ,
I tried to connect it with a potentiometer but i always get…
Part Number: TPS2411 Other Parts Discussed in Thread: UCD3138PSFBEVM-027 Tool/software: Good morning Mr. Shiven Dhir this is the question you had asked me some time ago .
"
TPS2411 is rated for 16.5V. Are you trying to scale down 600V to ~12V for…
Part Number: UCD3138PSFBEVM-027 Hi
I enabled a burst mode through GUI. And then click the "write to hardware",the input power was reduced.
Next, I click the "store ram to flash". Then the input power go back. Burst mode disabled.
…
Part Number: UCD3138PSFBEVM-027 Hello
I tested UCD3138PSFBEVM-027
At no load condition, there is no burst mode operation.
Sync FET is on PWM switching
How can I operate burst mode at light load.
Part Number: UCD3138PSFBEVM-027 Hi,
I tested IOUT_OC_FAULT_LIMIT function.
When I changed the value of IOUT_OC_FAULT_LIMIT, the function operated in normal.
But When I changed the value of IOUT_OC_FAULT_LIMIT under 5A , the IOUT_OC_FAULT_LIMIT operate and…
Part Number: UCD3138128A Other Parts Discussed in Thread: TPS2411 , UCD3138PSFBEVM-027 Tool/software: Good morning
sorry if I post this reply here I know it is not the right blog because it is about TPS2411 but I don't know how to go about answering the…
Part Number: UCD3138PSFBEVM-027 Other Parts Discussed in Thread: UCD3138 , Hello Is there a simulation model for the PSFB evaluation board (UCD3138PSFBEVM-027) of UCD3138? (E.g. LTSpice) Best regards.
Part Number: UCD3138PSFBEVM-027 Hello, is the main circuit on the UCD3138PSFBEVM-027 development board using a diode-clamped advanced phase-shifted full bridge?
Some documents say that the loss of the lagging type is smaller, why do you choose the leading…
Part Number: UCD3138PSFBEVM-027 Hello, When testing the primary 4-channel drive wave of UCD3138PSFBEVM-027, it is found that the 2-channel PWM of the fixed bridge arm QB1/QT1 is stable,
while the 2-channel PWM of the phase-shifted bridge arm QB2/QT2 is…
Part Number: UCD3138PSFBEVM-027 Hello Guys,
Good day.
How can one change the peak current mode control to a single loop voltage mode control of UCD3138PSFBEVM-027 ?
Thanks and regards,
Art