Other Parts Discussed in Thread: UCD7242 , PTD08D210W , UCD9224 , UCD74111 , UCD74120 , UCD7230 , PTD08A020W , UCD7411 , UCD9246 Hi,
Is it possible to make a 4 phase converter usingthe controller UCD 9224 and UCD 7242 fet? When I try selecting UCD7242 in fusion…
I assume the Fusion GUI is reporting an FLT when the rail is shutdown. This would be generated from the UCD7230 driver located on the PTD08A010W Module.
There are two sources for generating this response, there is a high side mosfet fast overcurrent protection…
Other Parts Discussed in Thread: UCD9240 , UCD7230 I am doing the dynamic test on the UCD9240 and UCD7230 combo design. The overshoot is higher than the required spec. I am trying to lower the overshoot and undershoot by adjusting the compensation parameters…
Could I ask what it is that you are planning to power with this dc/dc converter, what is the load?
What are your input voltage requirements for the DC/DC and what is needed for an output voltage and current?
The UCD7230 was designed to be used at higher…
Maher, There is a wide range of evaluation boards and reference designs for the C2000 MCU family. This page has a good summary of the various platforms.
The UCD7230 is a good choice for driving a synchronous buck regulator at these low frequencies. Of…
Dear Tom,
In my project ,power stage is controled by UCD7230. vin =15volt,double phase vout,FS=1MHZ,L=0.5uH,C=470uf*5+47uf*10,I want to get a adjustable Vout of 0 to 12volt. in the course of regulating, ofen burn down the low side MOSFET,ucd7230 is hot…
thanks for reply.
the issue has been fixed.
root cause: when the command of phase_info and store default all to carry out ,the ucd9240 will be reset.
solution: Add more decouple cap of 0.01uf near the power pin of UCD9240. It can guarantee PMBUS stability…
Hi,
1) Schematic page for the relevant UCD9248 attached below:
Configuration file for that part:
UCD9248 @ Address 52d Project.xml
Its the very first rail to start, so I'm fairly certain I have no voltage tracking turned on. If you need waveforms…
Other Parts Discussed in Thread: UCD9248 Hi,
We are working on a board with total of 8 UCD9248 controllers.
We have no issue to communicate with the devices through TI USB-GPIO adapter.
By setting the ONOFF CONFIG to Always Converting and also rely on…
Other Parts Discussed in Thread: UCD9248 We're bringing up a board with four UCD9248 parts. Excerpts from our schematics are available (privately) on request -- but it's a pretty standard design, borrowing verbatim from the Xilinx VC709 evaluation board…