Part Number: UCD90120 Hi,
I use I2C to read UCD90120A, but the CLK pulls down about 34ms during the transmission.
Should I adjust some settings about UCD9020A?
Thanks,
Owen
Part Number: UCD90120 Other Parts Discussed in Thread: UCD90SEQ64EVM-650 Context: due to supply chain issues, we were only able to secure stock of the UCD90120 (not A) so unfortunately we don't have the latest iteration of the product. I'm using Fusion…
Part Number: UCD90120 Other Parts Discussed in Thread: UCD90124 , UCD90124A , Hi Expert,
What is the diference between UCD90124 and UCD90120? Are they pin-to-pin compatable? I have checked the datasheet, that both devices are the same. Thanks!
Jimmy
Part Number: UCD90120 Hi Expert,
Pls advice Why there are 13 monitors pin in UCD90120,but support 12 rails only.
Best regards,
Eric Lai
Field Application Engineer
Texas Instruments Taiwan Limited
O: +886-2-2175-2582
M: +886-909-262-582
E-Mail:Eric…
Part Number: UCD90120 Other Parts Discussed in Thread: UCD90320 Hi,
I just had a question about this tidbit I see in the datasheets for the UCD90120 and UCD90320
The user configuration can be written to data flash using a gang programmer via JTAG or…
Part Number: UCD90120 Dear Expert
Could u tell me dsconnect R45, download OK, why no output ?
This is our shcemetic:
That's all three of them we configuration:
Part Number: UCD90120 Other Parts Discussed in Thread: UCD9081 , We are considering UCD90120 or UCD9081 for our new project. It is important for us to have small current consumption when device is in "Standby" mode (couple of mA). From the datasheet…
Part Number: UCD90120 Other Parts Discussed in Thread: UCD90320 , UCD90240 , UCD9090A , UCD90160A , I read this app note which says,
Another method to cascade multiple devices is to connect the power-good output of the first device to a MON/GPI pin of the…
Hi
I got your message and project file.
GUI 7.x stops supporting UCD90120 so the protocol is no long supported causing GPIO off. GUI 2.x is the only tool supporting UCD90120.
Regards
Yihe