Hi Yihe,
Thanks for the information.
yihe said: Are you sure 3V3 is connected to the UCD?
Yes, surely it was connected to UCD. There are other devices on the same rail like MSP430 which were all coming up when powered from other power source.
--
Regards…
Part Number: UCD90160 Hi,
I couldn't find any information on how to decode the UCD90160 top side marking, especially the Date Code marking.
Could you please help?
One example:
UCD90160
TI 31I
AF2Y G4
My guess it that 31I is the date code? how to…
Part Number: UCD90160 Hello expert,
My customer is fail on write 0xfb register and they would like to know why, do you have idea? Log is shown below.
#wedge_ucd_gpio_set 22 1 root@bmc:~# i2cset -f -y 2 0x34 0xfa 22 root@bmc:~# i2cset -f -y 2 0x34 0xfb…
Part Number: UCD90160 Other Parts Discussed in Thread: PMP9444 , , TPS65273V Hi TI team,
I have built an evaluation board with 2xUCD90160, 3xTPS65273V for my project and debugging with TI tools
My first issue is devices are not responding on GUI
my board…
Part Number: UCD90160 Hi TI Team:
We want to use watchdog function of UCD90160
Base on document “UCD90xxx Sequencer and System Health Controller PMBus Command Reference”, I need to configurate D3h
I want to configure GPI3 to WDI and GPIO16…
Part Number: UCD90160 Sorry, just getting back to this since we had a board spin. We updated our board with the UCD90160 for this spin.
The command line programming still does not work even though the script runner and full blown version do.
The fusion…
Part Number: UCD90160 Dear TI service team,
For this power management IC: UCD90160RGCR, I want to setup different triggered signal for power sequence on and off.
"For example, A signal need to be asserted when B signal is ready, and A signal need to be…
Part Number: UCD90160 Other Parts Discussed in Thread: TPS536C7 , TPS53681 Hi,
We have assembled UCD90160 device (Batch code: C5H0) in 5 boards. The device is not getting detected in any of the boards in Fusion GUI.
We have tried the following to debug…
Part Number: UCD90160
Hi Champs,
My customer is configuring UCD90160 as below to achieve a 1ms delay on a 10.2V undervoltage. However the the response time is much longer then expected. Could you kindly help to check the configurations?
GPIO2 Configurations…