Part Number: UCD90160A
Hello TI Team,
I am debugging a UCD90160A on a board that was already programmed before I received it.
I have two identical boards. Both boards originally responded at PMBus address 0x7E.
When power is applied, the…
Part Number: UCD90160A I am programming UCD90160A devices using a USB2GPIO with the Fusion Digital Power Designer software. Is there a way to clear the UCD90160A back to a "factory reset" so that it looks like a blank device when I connect to it? Tha…
Part Number: UCD90160A Tool/software: Hi TI Team,
I am using the UCD90160A Power Sequencer IC, Here we wants to check the LOGGED_FAULTS Register. For our application we want to reset all the registers while initial Power up. Followed the below sequence…
Part Number: UCD90160A Does the state machine for the UCD90160A PMIC have the ability to respond on the PMBus for the 10-bit Addressing and Reserved space? ex.
0x78-0x7B
10-bit addressing prefix
0x7C-0x7F
Reserved
Part Number: UCD90160A Other Parts Discussed in Thread: UCD90SEQ64EVM-650 , Tool/software: Hi Team,
I am using the UCD90160ARGCR as a power sequencer in my custom design. For hands-on experience, I have previously worked with the UCD90SEQ64EVM-650 evaluation…
Part Number: UCD90160A Tool/software: Hi Team, I am using the UCD90160A, In this UCD device my system input voltage is 12V, We are monitoring in the AMON Pin, If this 12V goes to the 10V, System Power rails to be turned off, while its come up above 10V…
Part Number: UCD90160A Tool/software: UCD90160A: STATUS_VOUT in the project file shows faults and warnings in some channels
1.
I have inherited the project file (.xml) set up for voltage monitoring in 13 out of 16 channels. No GPIO configured as they…
Part Number: UCD90160A Other Parts Discussed in Thread: UCD90160 , We have the UCD programmed to use the System WD reset feature. (if the micro doesn't strobe the UCD, the UCD will generate a system reset on the microprocessor) We have used the UCD90160…
Part Number: UCD90160A Other Parts Discussed in Thread: UCD90160 Tool/software: Is there a good method to migrate the XML File from UCD90160 to UCD90160A without loading onto a UCD9016A device.
We are migrating our designs and do not currently have…
Part Number: UCD90160A Tool/software: Hi Team,
I am currently working with the UCD90160A device and have successfully tested its watchdog functionality. As per our system requirements, we need to disable the watchdog during U-Boot execution and re-enable…