Part Number: UCD90160A Dear Ti
Could you tell me something, question of the following.
Does UCD90160A need external Flash memory ?
How to set the GPIO status of UCD90160A ?
Can I control and program UCD90160A through SMBus ?
If there has any question…
Part Number: UCD90160A Question about "Fusion Digital Power Designer" (aka FDPD) - no access to "Export" function
Details:
Have FDPD version 7.7.1 installed, USB Adapter attached (firmware rev 1.0.11) but UCD90xx device is NOT connected…
Hi
For the rail that UCD doesn't control, the only thing I can see is that if they are the sequencing off dependencies of other rails, it may prevent the power down of other rails since those aux rails never below POWER_GOOD_OFF threshold due to the control…
Part Number: UCD90160A Hello,
I created a Ti support request ticket, but it has been unanswered for 5 days now, so I'm asking for assistance here. The issue I'm having is with the Digital Designer GUI software, for programming UCD90160A. I think the problem…
Part Number: UCD90160A Other Parts Discussed in Thread: UCD90320 , UCD9090A , UCD90160 I have questions about 2 different UCD90xxx Features
Feature 1: Alert Signal
On a system with 2 UCD90160s, we see the ALERT signal (combined from both devices) from the…
Part Number: UCD90160A Dear team,
We want to do field side code upgrade of UCD90190A.
To implement this feature, we need UCD device can work normally with original code config during system power on and re-load new config once next power on cycle.
Is…
Hi
No, if the checksum of UCD90160A is wrong, when launched GUI, it reported that the device does not have valid configuration.
i do not think that's the case here.
Regards
Yihe
Part Number: UCD90160A Other Parts Discussed in Thread: UCD90124 Hi Team,
My customer asked the following question on getting started with the UCD90160A:
The eval I got had a ucd90124, and I replaced it with ucd90160a because its what I placed in my…
Part Number: UCD90160A Dear team,
We face to an issue about control rail#1 on/off. Our target is pull GPI to low to turn off rail#1 after system power on.
To double confirm the issue, I have change from "control pin only" to "operation only" and turn…
Part Number: UCD90160A Hi TI FAEs
We'd like to shutdown rail (Rail 16) via GPI#1, how to I set the configuration by GUI?
we've set GPI#1 as fault enable and fault shutdown rail but the rail not shutdown when GPI#1 (we called PWR_CYC_ALL_N be set to…