Other Parts Discussed in Thread: UCD90120A , UCD9090 , UCD90160A , UCD90160 , UCD90240 , UCD90320U , UCD90120 , UCD9090A , UCD90124 , UCD90124A , UCD90320 The re-sequencing count is reset when all re-sequencing rails stay above the POWER_GOOD threshold for more…
Other Parts Discussed in Thread: UCD90120A , UCD9090 , UCD90160A , UCD90160 , UCD90240 , UCD90320U , UCD90120 , UCD9090A , UCD90124 , UCD90124A , UCD90320 Each monitor rail has its Vout Exponent, which limits the maximum voltage the device shall return. Make sure…
Other Parts Discussed in Thread: UCD90120A , UCD9090 , UCD90160A , UCD90160 , UCD90240 , UCD90320U , UCD90120 , UCD9090A , UCD90124 , UCD90124A , UCD90320 Yes, but it is not recommended to do so. A rail EN pin has many features that logic GPO pins do not have, such…
Other Parts Discussed in Thread: UCD90120A , UCD9090 , UCD90160A , UCD90160 , UCD90240 , UCD90320U , UCD90120 , UCD9090A , UCD90124 , UCD90124A , UCD90320 No. A data flash image file can only be generated from a live device or a data flash script file. When offline…
Other Parts Discussed in Thread: UCD90120A , UCD9090 , UCD90160A , UCD90160 , UCD90240 , UCD90320U , UCD90120 , UCD9090A , UCD90124 , UCD90124A , UCD90320 V33A supplies power to voltage reference and ADC blocks inside the device. A large ripple on V33A can affect…
Other Parts Discussed in Thread: UCD90120A , UCD9090 , UCD90160A , UCD90160 , UCD90240 , UCD90320U , UCD90120 , UCD9090A , UCD90124 , UCD90124A , UCD90320 The names of rails, GPIs, and logic GPOs are stored in the local PC instead of the respective devices. Therefore…
Other Parts Discussed in Thread: UCD90120A , UCD9090 , UCD90160A , UCD90160 , UCD90240 , UCD90320U , UCD90120 , UCD9090A , UCD90124 , UCD90124A , UCD90320 The Invalid Logs flag is cleared only on the next boot up if the device does not see any corrupted logs. The…
Other Parts Discussed in Thread: UCD90120A , UCD9090 , UCD90160A , UCD90160 , UCD90240 , UCD90320U , UCD90120 , UCD9090A , UCD90124 , UCD90124A , UCD90320 The "time between re-sequences" only starts to count when all rails are below their POWER_GOOD_OFF thresholds…
Other Parts Discussed in Thread: UCD90120A , UCD9090 , UCD90160A , UCD90160 , UCD90240 , UCD90320U , UCD90120 , UCD9090A , UCD90124 , UCD90124A , UCD90320 Decoupling capacitors on MON pins are recommended. MON pins are ADC channels. There is no internal filtering…
Other Parts Discussed in Thread: UCD90120A , UCD9090 , UCD90160A , UCD90160 , UCD90240 , UCD90320U , UCD90120 , UCD9090A , UCD90124 , UCD90124A , UCD90320 Although it is optional, it is always recommended to have a PMBus connector to connect the Fusion GUI. You…