Part Number: UCD9081 My UCD9081 is keep on Resetting my system. I want to understand what is going wrong on the device.
Expecting to have a call to review the design.
Part Number: UCD9081 Hello,
I am trying to organise production programming of this sequencer, and can export a .hex file, but can't work out which tool I should be using to program the sequencer.
My only real goal here is to great a file which can…
Part Number: UCD9081 Hi,
When I push on "Discover Devices" in the UCD9081 EVM GUI, I get a reset to the sequencer.
How could I use this "Discover Devices" without to reset the sequencer?
I have a primary sequencer and seconded sequencer…
Part Number: UCD9081 Hi,
I want to use several UCD9081 for a system that connects each UCD9081 to each DSP.
How do I initiate power down sequence to one of UCD9081 for one DSP, while the all systems are working?
1. could I use one Mon input of UCD9081 for…
Part Number: UCD9081 Hi,
I'm using UCD9081 in my design with the UCD9081 EVM software w/o any problem for a while. Recently I made quite a few changes to the design (i.e. configuration) and after a configuration upload, the device has stopped responding…
Part Number: UCD9081 hi,
UCD9081:
When are the address lines sampled? Before before reset line go from "0" to "1" or after reset line "0" to "1"?
and what is the hold time sample for the address line read?
Part Number: UCD9081 Hi,
When I build the footprint, how much deflection is allowed at the pad of pin in mm?
For example if the PAD pin footprint in the datasheet is 0.6x0.24mm could I build 0.7x0.27mm?
Part Number: UCD9081 Other Parts Discussed in Thread: UCD9090A
Hi,
I do some tests on the UCD9081 EVB. Further to what we talked about use UCD9081 for two separate device.
I was succeed to shutdown device_1 (EN1, EN2, EN3, EN4) with fault with FET on MON1…
Part Number: UCD9081 Hi,
I want to use ucd9081 for power up and down 2 devices. which device are using 4 EN and 4 MON separately.
device_1 (MON1,MON2,MON3,MON4,EN1,EN2,EN3,EN4) device_2(MON5,MON6,MON7,MON8,EN5,EN6,EN7,EN8)
my Q is: if I what to shutdown…
Part Number: UCD9081 Hi Experts!
Can someone provide the maximum rated junction temperature and the ESD ratings for this device?
I don't see max operating junction temperature anywhere in the datasheet.
There is a note in the datasheet that the ESD…