Part Number: UCD9090-Q1 Other Parts Discussed in Thread: UCD9090 Hello,
I would like to know the feature size of the UCD9090-Q1, are we talking about 180nm ?
Also, is the FLASH based on NOR technology ?
Best regards,
Clément
Part Number: UCD9090-Q1 Other Parts Discussed in Thread: UCD9090 Hello,
Is it possible on an embedded application to perform a CRC check of the FLASH and RAM of the device while it's running nominally.
I didn't see any commands allowing that in the…
Part Number: UCD9090-Q1 Tool/software: Hi,
We are currently trying to pre-design a new board and I am investigating the power consumptions to define the DC/DC needs.
In the datasheet, only nominal consumption are provided, how can we work out a maximum…
Part Number: UCD9090-Q1 Tool/software: Please show how to activate ENABLE_ACTIVE_TRIM using Fusion GUI, I can't find it in GUI. I would like to use it to adjust the output through VOUT_COMMAND.
Part Number: UCD9090-Q1 Tool/software: Hi Team,
With 2x UCD9090-Q1 in the system, the PMBus_ADDRx resistors are as follows:
Device 0:
Expected Address: 0x34
PMBus_ADDR0: 31.6kOhm
PMBus_ADDR1: 31.6kOhm
Device 1:
Expected Address: 0x41 …
Part Number: UCD9090-Q1 Tool/software: I have some DC-DC power regulator needs and I was hoping TI could recommend the best DC-DC non-isolated match. The input will be +5V.
0.88V, 25A, 3%(1%DC accuracy + 2% AC ripple) , step response 9A over 350ns…
Part Number: UCD9090-Q1 Other Parts Discussed in Thread: UCD9090 Tool/software: Hi TI Expert,
I'm using the UCD9090 in my automotive application. I’ve measured the I2C bus and found that the falling time does not match the datasheet specifications,…
Part Number: UCD9090-Q1
We are using UCD9090-Q1 device in our system. The connection involves enabling voltage rails and monitoring them. The voltage rails have warning and fault thresholds defined to be +/-10%. All actions on fault are disabled, therefore…