Part Number: UCD9090-Q1 Hi Team,
Can we use the PORz_OUT (3.3V) from the AM62 as an input into the UCD to let it know that AM62 is on and ready for other items to be turned on?
Is there any issue with this?
Thank you,
Delaney
Part Number: UCD9090-Q1 Other Parts Discussed in Thread: UCD9090 Hi, I'm now working on UCD90XXX series chips for Xilinx FPGA power sequencing.
I have read the datasheet of ucd9090-q1、" Fusion Digital Power Designer GUI 7.0 for the UCD90xxx Sequencer…
Part Number: UCD9090-Q1 Just want to make sure i understand how to read MON11 for UCD9090-Q1.
Based off of this link it sounds like you can only read MON11 as current or temperature ( link ). Is that true?
Assuming that is true then they just need to follow…
Part Number: UCD9090-Q1 Other Parts Discussed in Thread: UCD9090 , UCD9090A Hi team,
I am Currentaly using UCD9090A TI part in our drsign. Due to long lead time, i have choosen UCD9090-Q1 as an alternaye part of UCD9090A. I have mounted the UCD9090-Q1…
Part Number: UCD9090-Q1 Other Parts Discussed in Thread: UCD9090 , TPS38700 Hi Team,
Can you checknmy understanding?
For all GPIO configured as an output enable, is that a timing UCD9090 float before UCD9090 reset? Should we add the weak pull low?
Thank…
Part Number: UCD9090-Q1 Hello TI team,
Is it possible to configure power-down sequencing of the UCD9090-Q1 device without using the CONTROL pin or the OPERATION command? Currently I am using the "Auto Enable" option for power sequencing, but it seems…
Part Number: UCD9090-Q1 Hello TI team,
After powering up the UCD9090-Q1, during the start process of TI Fusion Designer I get the following error:
If I click yes I can operate the device normally. As soon as I power cycle the device, the configuration…
Part Number: UCD9090-Q1 Other Parts Discussed in Thread: UCD9090 It looks as though the UCD9090 allows for reading all MON rails at once or specifically for which rail you want to measure based on data in this document here: https://www.ti.com/lit/ug/slvu352g…
Part Number: UCD9090-Q1 Other Parts Discussed in Thread: UCD9090 Hi Team, Our customer is currently using UCD9090. Is it possible to monitor an 11th voltage rail using the Fusion GUI? Section 7.4.3.1 of the datasheet says it can monitor up to 11 voltages…
Part Number: UCD9090-Q1 Hello.
We already using the UCD9090RGZT, and there is no stock of it. Can we use the UCD9090-Q1 part instead with the same flash (take the flash code of UDC9090 for the the -Q1 device version)?
Or we have to generate a new flash…