Part Number: UCD90SEQ64EVM-650 Other Parts Discussed in Thread: UCD90124 , UCD90160 Tool/software: I purchased the EVM module and by default the TI Fusion GUI is detecting the device as UCD90124.
As per the description of the EVM it includes all the various…
Part Number: UCD90SEQ64EVM-650 Hi,
For this eval board when we supply the 5V DC input power provided by the USB interface there is no output voltage available on the GPIO pins on the board. We then tried to supply the 5V using the J5(Screw Jack) and once…
Part Number: UCD90160A Other Parts Discussed in Thread: UCD90SEQ64EVM-650 Dear TI engineer,
I installed UCD90160A into XU1 and found that the variation of READ_VOUT is large. I connected ADC output from another ADI EVB board EVAL-AD5675SDZ to MON1 or…
Part Number: UCD90SEQ64EVM-650 Other Parts Discussed in Thread: UCD90124A , UCD90124 Hello Team,
For the power sequencing, I have started to work with UDC90124 in the UCD90SEQ64EVM. I have made a power sequence in fusion design online.
I have some point…
Part Number: UCD90SEQ64EVM-650 Other Parts Discussed in Thread: UCD90124 , UCD90124A , UCD90120A , UCD90160A , UCD90160 , UCD90120 I am trying to use the Eval board I just bought.
It has a UCD90124 installed.
It can read the ID as 104.
But the part selector…
Hi
Please submit new post for each individual question so that the whole community can be benefited instead of making a long post.
For your case, you have to set the rail's ON_OFF_CONFIG to OPERATION MODE. you can turn on or off each rail via operation…
Part Number: UCD90SEQ64EVM-650 Other Parts Discussed in Thread: USB2ANY
I have a customer using UCD901XX to sequence power for FPGA.
The FPGA is also connected to the UCD PMBus for operational control and monitoring of rails after boot.
Customer uses…
Part Number: UCD90SEQ64EVM-650 Other Parts Discussed in Thread: UCD90120A , MSP-TS430PEU128 I am prototyping some MSP430 code to interface with a UCD90120A device via eUSCI_B I2C. I have access to a UCD90SEQ64EVM-650 board with a similar UCD90120A device…
Part Number: UCD90SEQ64EVM-650
Hi everyone,
I bought a kit developement board UCD90SEQ-650. Before it operated good, but now when I connect usb to PC a green light ( USB atttach) isn't on. And PC notify Unkown device. Please help me fix that! Thank you…