Part Number: UCD91320 Hi team,
My customer is evaluating UCD91xxx. Please help clairfy below questions. Thank you.
The deviation between UCD-POWER-SEQUENCER-STUDIO and UCD-POWER-SEQUENCER-STUDIO-DESIGN? The former can be accessed.
Can UCD91xxx…
Part Number: UCD91320 Hi,
What is the minimum current that can be sourced/sink on the Enable pins? I see that Maximum allowed current sunk or sourced by device pin is 6mA.
The main question is if I can enable my regulators directly or if I need to…
Part Number: UCD91320 Other Parts Discussed in Thread: UCD90320
What is the supply current for the device UCD91320?
In the datasheet and product page the following information are available:
Iq : 10mA
IDDERASE : 10mA
IDDPGM : 10mA
I(ADC) …
Part Number: UCD91320 Hi Team,
Our customer is currently evaluating the UCD91320 and would like to know if it supports configuration updates via PMBus?
The customer's host platform is running Linux 6.x and communicates with the UCD91320 via PMBus…
Part Number: UCD91320 Hi, I need some information on this UCD91320 chip in regards to CLI automation for programming the chip and read and write the GPIO's, device id etc on this chip. I have read some documents and could not find any specific information…
Part Number: UCD91320 Hi team,
Please provide information regarding the VREF+/- pins.
When using an external VREF, should the VREF- pin be left open or connected to GND? Leaving J1 open—as described in the EVM documentation—results in VREF- also being…
Part Number: UCD91320 Using the Sequencer Studio software tool, I'm having difficulties in defining the sequencing On and Off phases. I've defined all the rails and have entered the On and Off dependencies and Fault Slaves.
There are 22 voltage rails…
Part Number: UCD91320 Hi Team,
Currently using UCD91320 for voltage margining
How should the following parameters be set?
VOH : ?
VOL : ?
F_CLK : ?
When adjusting the voltage margin, should we use DPWM VOH or DPWM duty cycle?
According to…
Part Number: UCD91320 Hello,
I2C can get stuck/hung up by downstream devices sometimes. Is there a way to reset the I2C communications without resetting the whole IC?
Nick