Part Number: UCD9240 Hi
My customer has some queries need help.
They use UCD9240 to control the following modules, which are: Rail 1: PTD08A020WAD, designed to output 1V0; Rail 2: PTD08A010WAD, designed to output 2V5; Rail 3: NA; Rail 4: PTD08A020WAD, designed…
Part Number: UCD3138 Other Parts Discussed in Thread: UCD9240 Dear friends,
I have following questions regarding the Digital Controllers UCD3138 and UCD9240.
1. What are the significant features and advantages of UCD3138 over UCD9240?
2. Which controller…
Part Number: UCD9240 Anyone have v2.0.89 installation media? Looking to import a device configuration from project file (.xml). Not able to do so due to the new GUI and unfamiliarity with the new version I have installed.
Thanks!
Other Parts Discussed in Thread: UCD9240 , UCD7230 Hello
I am trying to play with UCD9240 on PR662F prototype board.
I am able to connect and configure the device via TI I2C dongle and TI Fusion Designer.
The only problem I have is unstable READ_IOUT values…
Other Parts Discussed in Thread: PTD08A010W , UCD9240 , UCD7230
Dear Sir,
I have tried to make a board with UCD9240 & PTD08A010W for the power supplies.
For the 1st trial, I've tried to configured a rail #1 to 1.2V. After setting the Configuration…
Other Parts Discussed in Thread: PTD08A010W , UCD9240
Dear Sir,
I have a trouble to use the power module PTD08A010W that is controlled by UCD9240.
I've tried to make a PCB board with a power circuit as below. It refers to a Xilinx SP605
demo board…
Other Parts Discussed in Thread: UCD9240 Time progress of the electric power under FPGA operation, voltage, and current was acquired using UCD9240 and a Fusion Digital Power Designerl. 1~2% of error arises in the value of the acquired electric power value…
Other Parts Discussed in Thread: UCD9240 Is it possible to compensate for delivery droop with the UCD9240?
There is a known amount of resistance (8mOhm) between my measurement point, and the load. The supply is 1V, and the amount supplied is between 1A…
Other Parts Discussed in Thread: PTD08A010W , UCD9240 Hi,
I am facing trouble with UCD9240 module in Xilinx SP605 evaluation board. It was working comfortably, but at some point of time it stopped powering up FPGA. The FPGA is powered by UCD9240 and PTD08A010W…
Other Parts Discussed in Thread: UCD9240 , PTD08A020W , PTD08A015W Hi,
I have been developing an ADC board based on the design of Xilinx ML605 demo board. The power supply circuit is also nearly the same as ML605 using 2 UCD9240 with 5 PTD08A020W and 2 PTD08A015W…