Part Number: UCD9246 Other Parts Discussed in Thread: LM57 , LM94022 , UCD74120 We would like to use the LM57-10 to measure the board temperature of our UCD9246 based design. This will be fed directly into the "TEMPERATURE" pin, w/o a mux.
Fusion…
Part Number: UCD9246 The library manager inside Fusion Digital Power Designer allows entry of the tolerance for the output capacitors.
How is this tolerance factored into the calculation of the compensation coefficients?
I've reviewed SLUU490 and the…
Part Number: UCD9246 What is the duty cycle of the SYNC_OUT signal?
I am having to design an AC coupled level shifting circuit that will be driven by SYNC_OUT and need to understand its duty cycle. Thanks.
Part Number: UCD9246 Other Parts Discussed in Thread: UCD9240 Hello,
One of our customers is experiencing the following problem. Any troubleshooting steps are appreciated! Let me know if you need more info:
" We use two UCD9246 with each chip controlling…
They should be able to just stick with the script order as generated from the Fusion GUI.
As for failing with the default script, the only thing I can think of is that the V33 voltage rise on the controller may too slow, possibly resulting in the NACK of…
Our application requires extremely small size/power density.
We are using 1 MHz/3 phases for a core FPGA supply, and I agree that with a non-digital current-mode controller I could achieve much better active transient response.
As it is, I'm getting about…
Part Number: UCD9246 Other Parts Discussed in Thread: LMZM23601 , LP5907 Is there any concern about using a buck converter to supply V33A, V33D, and V33DIO of the UCD9246? I have a LMZM23601 providing 3.3V on the board, and for simplicity and efficiency…
Part Number: UCD9090 Other Parts Discussed in Thread: UCD9246 , Our company (phyton.com) produces device programmers for mass production and engineering and support programming for a variety of TI devices (ARM Cortex, C2000, MSP430 and others). We have…
Part Number: UCD9246 Hi,
I would like to upgrade the firmware of UCD9246, so to be able to program the data flash in 'Normal mode' instead of 'ROM mode'.
The document "Configuration Programming of UCD Devices" states that fw version…