Part Number: UCG28826EVM-093 Tool/software: We understand this IC is optimized for 60Hz AC source rectified into DC. Can it be used in DC from 400Hz AC? Can we use the eval kit with 400Hz AC? What do we need to change?
Part Number: UCG28826EVM-093 Tool/software: Dear Sir ,
We are doing design USB-C PD power adapters at 100W and studying with UCG28826EVM-093.
to save time in design is possible can you please share me schematics and PCB files for the EVM
thank…
Part Number: UCG28826-CALC Other Parts Discussed in Thread: UCG28826EVM-093 Could you share the UCG28826EVM-093 PCB Altium file? We wants copy the EVM layout to build the board. Thanks
BR,
Gary
Part Number: UCG28826EVM-093 Other Parts Discussed in Thread: UCG28826 Tool/software: Hello team,
Do we have any reason the UCG28826 EVM uses transformer which has "SHIELD"?
Best regards,
Shotaro
Hi Gaston,
Yes, you can tune feedback resistor divider to get 29V output voltage in PMP41145 reference design, keeping limit of 65W output power. But in UCG28826EVM-093 evaluation module you cannot do that as used PD controller WT6636F support USB PD…
Part Number: UCG28826-CALC Dear Srs
Transformer reference RLTI-1464 (RENCO): I can't find datasheet, could you send it?
Thermal test: how did you test it: open air or inside a plastic box?
best regards
raimon ribal
www.simonelectric.com
Hi Gary,
During burst mode, VCC do not drop and as mentioned earlier this device is self-biased and will maintain required VCC throughout the load. For your reference, please see below waveforms taken on UCG28826EVM-093 (), in burst mode VCC is regulating…
Hello,
We have a few different reference designs around this power level/output.
65W GaN Flyback
PMP41145
UCG28826EVM-093
140W GaN AHB
TIDA-050074
Best,
Kyle Wolf