Part Number: ULN2003A hi,
We are facing issue with the crosstalk. 1.As shown in picture attached first DO is properly driving the load realy (coil resitance 125 ohms) and realy was energised properly. 2. Driving Second DO is not driven properly and…
Part Number: ULN2003A 7.4.2 Resistive Load Drive When driving a resistive load, a pullup resistor is needed for the ULN2003A device to sink current and to be a logic high level. The COM pin can be left floating for these applications. I don't understand…
Part Number: SN74HC373 Other Parts Discussed in Thread: ULN2003A , , TPL7407LA , TLC6C598-Q1 I apologize for just confirming this. I'm using the SN74HC373 and ULN2003A to control LEDs, and each channel is about 20mA. 1. According to the graph in Figure…
Part Number: ULN2003A
Team,
Could you help with this application issue! PLease find the detailed slide below. thanks.
ULN2003A IC Troubleshooting - Read-Only (1).pptx
Part Number: ULN2003A hi team,
my custoemr used ULN2003A for servel yeras. Recently they found that the ESD of products using the newest ULN2003A can't pass the 8kV ESD test.
Do we have any changes in the ESD performance of new ULN2003 device? Do…
Part Number: ULN2003A Tool/software: Hi Team,
My customer is asking for the TINA Library of ULN2003A
Could you please provide the link? or tell me where can I find it?
Thanks a lot!
BR,
Jenny
Part Number: DRV8421 Other Parts Discussed in Thread: ULN2003A Hello team,
Can you prepare a graph for "Maximum Collector Current vs Duty Cycle" like ULN2003A?
My customer is considering to apply DRV8421A instead of transistor array like ULN2003A…
Part Number: ULN2003A Hello team,
My customer is thinking migration to DYY from PW. We think thermal metric of DYY should be OK. But as a back up plan, we want to know a way to close to PW.
Do you have any idea?
Are we able to use a heat dissipation…
Part Number: ULN2003A
Hi all,
We are using this device to drive an actuator on an indoor unit control board.
We are considering an actuator with a coil resistance of 55 orm (the typical actuator used so far has 100 orm coil resistance).
-Voltage…