Hello,
The Webench coil designer currently gives a "CAD export was not completed successfully." message when we try to export design to CAD:
We've tried: - Exporting to a different software (cadence, allegro, altium, etc) - Clearing browser…
Hello,
The Webench designer will generate a schematic and BOM for your design. In regards to the UCC38050, I believe it will generate a boost stage for you based on an 85-265V AC input with roughly a 390 V output. You would then have to step that voltage…
Hi Jonathan,
Understood. I would utilize the Design Calculator to cross reference your components selection for your power levels and Vin range. I can help with that if you provide VIN range (min and max, AC or DC), fsw at full load, Output power. Please…
Part Number: WEBENCH-POWER-DESIGNER Other Parts Discussed in Thread: TPS53647 I miss the old Webench application where you could fully customize your design in the schematic editor. I want to be able to really go full Frankenstein and experiment with different…
Part Number: AM625 Other Parts Discussed in Thread: SK-AM62 , SK-AM62-LP , TPS65219 , SK-AM62B-P1 1. We are working on design of AM6254 Processor and we need to give POE & 12 Volt DC Jack as input power source and NOT Type C USB.
So We have checked both…
Part Number: MSPM0G3507 Hi,
My customer is using FreeRTOS on MSPM0G3507.
It needs low power mode (standby1) in the most running time and wake up by a period 50ms timer.
There is no low power mode example of freeRTOS in the MSPM0 SDK.
During studying,…
Part Number: LM5156 hi sir
i would like to design a dc-dc power stage, spec as below, LM5156 is a right solution?
For Positive, +10V~+110V Vout programmable, 48Vin, Continuous 0~40V /2A, Transient 110V/2A
For Negative, -10V~-70V Vout programmable, 48Vin…
HI Snigdha,
thank you for checking our reference designs.
Yes, this design matches very closely the parameters you have given above.
As I am not an expert on the PSE POE I really can not judge if this will provide all the required parameters for this…
Part Number: LM5116 Hi, I have designed a 12V/20A power supply with an LM5116 controller. I am able to obtain the output voltage, but the output inductor heats up as soon as I power up the board(Under no load condition). I have used the component values…