We are using kernel 5.10.72. This option is present in some documentation and also posts on this forum, for example:
https://community.nxp.com/t5/i-MX-Processors/Step-by-step-How-to-setup-TI-Wilink-WL18xx-with-iMX6-Linux-3-10/m-p/452922
https://e2e.ti…
Other Parts Discussed in Thread: WL1801 Hi all,
I've previously had support from this forum in getting the WL1801 up and working with a Zynq 7000 processor running Linux, but recently I've noticed some weird behaviour when attempting to use the WiFi and…
Other Parts Discussed in Thread: WL1835 , WL1801 Hi ,
According to WL18xx_WLAN_Hardware_Design_Guide ,a 10K pull up on IRQ pin will enable Debug mode. So i would like to know if we are using Debug mode any other functionality will have impact.
Thanks
Naigin…
Other Parts Discussed in Thread: AM3354 We are looking at using a wilink8 based wifi module, attached to our am3354 which has a real time clock. Ideally, we would like to avoid having a separate 32khz oscillator, and to just use the RTC oscillator that…
Hi Nick,
No. CC3235 devices cannot work with external PA or FEM (WLAN Front-End Module) because there internal RF switch for 2.4GHz path.
But I am not 100% sure about WL1801, WL1831 chips because there is no official datasheet on web.
Jan
Other Parts Discussed in Thread: WL1801 , WL1271 Hi,
We've designed a custom board around the Xilinx Zynq processor including the WL1801. The WL1801 is connected to the Zynq through the SDIO interface. We're trying to bring up the device and not having…
Other Parts Discussed in Thread: WL1801 , WL1835MOD Hello TI,
My customer is making the footprint for the WL1801. The datasheet is quite confusing to us. On page 5, Figure 4-1 says it is a Bottom View. To us, it looks as if it should be a top view. i.e…
in AP MODE(am3352-wl1801), it seems have no problem. but in STA MODE(am3352-wl1801), if the board(am3352-wl1801) close to AP(iptime N5-r1) about 5 cm. it works fine, then the board(am3352-wl1801) move away from AP(iptime N5-r1) about 1 M. then beacon lost…
Other Parts Discussed in Thread: WL1801 Hi, my previous problem not solved, but i can test my board with smartphone.
place my board close to AP. (about 5 cm).
i am testing some network middleware with smartphone app.
sometimes, i think my board seems to…