Other Parts Discussed in Thread: WL1801 , AM3352 Hi. I am using AM3352 based board (evmsk) with wl1801 WiFi module with kernel 3.12.
WiFi module is connected to cpu through mmc2 , 2 gpio for wl_en, irq .
problem is :
am335x-evm login: root root@am335x-evm…
Other Parts Discussed in Thread: WL1801 Hi, how i can switch between ap and sta mode?
to get my router ssid, have to start wl1801 as ap mode.
then if i try to switch sta mode, i get follow error message:
root@am335x-evm:~# iw wlan0 connect my_router_…
Other Parts Discussed in Thread: WL1801 For WL1801 module, we need Test Reports covering following standards:
1. EN60950 2. EN62311 3. EN 301 489-1 4. EN 301 489-17 5. EN 300 328
These reports are not public according to this thread:
http://e2e.ti.com…
Other Parts Discussed in Thread: WL1801 , WL1831 Hi!
I have a question about WL1801/WL1831 (150 Mbps versions of WiLink).
Does anyone know what the real world maximum UDP throughput is for them?
I can only find figures for the 300 Mbps version.
Thanks! …
Other Parts Discussed in Thread: WL1801 We have wl1801 chips and want to make the wifi application base on another samsung ARM A8 platform.
On android4.0, I'm looking for a suitable porting guide for wl1801 chips,but seems failed.
It seems all kinds…
Dear Marco & Victor,
Is this issue resolved.
I am also using TI's Wilink8 package with DM8148EVM also getting the crash dump as below:
----------------------------------------------------------------------------------------------------------…
Hi Rasmus Ahiberg,
We checked 26MHz clock signal to wifi module and fix this issue successfully. At this time wifi module can scan network.
Thanks so much for your reply.
Other Parts Discussed in Thread: WL1801 Is there a plan for an evaluation module for the WL1801? Will it be able to connect easily to the Sitara SK EVM?
Part Number: WL1835MOD Other Parts Discussed in Thread: WL1801 Is there a register in the WL18xxMOD family of parts that can be read from using a micro to detect what WiLink chip is present? I may have to use a different GPN from the current one in my system…
Hi Naveen,
We have the WL1801 and WL1831 devices on TI.com ( https://www.ti.com/product/WL1801 ). You can request access to the collateral which includes the reference design on the product pages.
Chip-down devices do not come with certification, so you…