Part Number: WL1807MOD In changelog for firmware 8.9.1.0.3 I can read:
- fix a FW crash at IntMemBlockErr(). It is triggered only in management frames transmission case. - long management frames include RRM report for example. It is highly advised to…
Part Number: WL1807MOD
Hi, We want to enable the hostapd in 2.4GHZ wpa3. Below are the configuration details. hostapd is not enabled. Please let me know what is the mistake iw dev wlan0 interface add wlan1 type __ap ip addr add 192.168.10.1/24 dev wlan1…
Part Number: WL1807MOD
Problem Statement
The LCC is experiencing frequent Wi-Fi disconnections while connected to the THERMOS wireless network.
The THERMOS SSID is configured as a mesh network and is broadcast on both the 2.4 GHz and 5 GHz bands…
Part Number: WL1807MOD Hi Team,
one of our customers is experiencing issues with the registration of our devices mounting the WL18MODGI wifi module, in Korea.
The regulatory office is requesting not only the KC RF report and the KC registration (both…
Part Number: WL1807MOD Tool/software: I installed the TI software (TI Wireless tool 4.0.0.2) for communicating with the WL1807MOD. So far I am not able to connect to the module. I have taken pictures for the error, but can not find an option to up load…
Part Number: WL1807MOD Tool/software: Hi,
We're proceeding with wifi alliance certification for our product.
as part of it, we're using quicktrack tool. As many versions are available as per wifi-allience forum, we wish to know which version is…
Part Number: WL1807MOD Other Parts Discussed in Thread: WL1837MOD
Team, Question is related to the below post: https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/1514228/wl1837mod-wl1837modgi
The WL1837MOD seems to have…
Part Number: WL1807MOD Hi,
We are using the WL1807MOD GIMOCR module with a single antenna. The chip is connected in 802.11n (40 MHz) mode on the AP, and the SDIO clock on our board is set to 37.5 MHz . Despite this, we are only seeing about 30 Mbps…
Part Number: WL1807MOD Hi,
We are using the WL1807MOD GIMOCR module with a single antenna. The chip is connected in 802.11n (40 MHz) mode on the AP, and the SDIO clock on our board is set to 37.5 MHz . Despite this, we are only seeing about 30 Mbps…
Part Number: WL1807MOD Other Parts Discussed in Thread: WL1837MOD Tool/software:
5.2.5 – Fail: The test case was ran three times and all three times failed at step 3. The throughput was too low.