Hi Lei,
We have identified the issue and are working on a timeline when we can officially release the fix.
Prior to making an official release of the firmware, we need to ensure it's passing our internal tests.
We will update you on the timeline soon…
Hi Jeremy,
1. I am not sure of the exact parameters you need to specify to ensure connection to the Sony headset. TI does have access to this headset on a remote site.
2. HCI_Setup_Synchronous_Connection could potentially overwrite the latency value specified…
Part Number: WL1831 Hi,
We have an issue where one of our devices in the field is unable to connect to a wifi network on our device running a WL1831 chip. All we've been able to work out is that the authentication is timing out. The wifi network is a…
Part Number: WL1831 Hello
WL1831GYFVT
Our customers have some failure cases in FFD test in WiFi certification.
Any suggestions?Attached is the report. Fail_FFD.zip
Part Number: WL1831 Hi Champs,
What is the maximum data rate of BLE inside the Wilink device?
The data sheet says it is Bluetooth 5.1 secure connection compliant but doesn't mention BLE.
Regards,
Kien Nguyen
Part Number: WL1831 Hi Champs,
WL1831 can operate up to -40C (i.e. Industrial temperature), whereas at module level (i.e. WL1831MOD) can only operate up to -20C. Which circuit/part limits the temperature performance?
Do notice that only WiLink 8 modules…
Part Number: WL1831 I have a customer who is new to the wireless space and could use some design suggestions.
The application includes several nodes all communicating to one central node independently of any existing network.
A few initial questions from…
Part Number: CC2564C Other Parts Discussed in Thread: WL1831 Hi, we are trying to replace our old BT controller WL1831 with CC2564C, our board is based on a Jacinto running Android 8.0. Do you have an integration guide that can help us with this task…
Part Number: WL1831MOD Other Parts Discussed in Thread: WL1831 The Bluetooth driver of wl1831 is loaded successfully after transplanting BlueZ on our Linux platform. Using Bluetooth CTL tool can make wl1831 search for Bluetooth of other mobile phones,…
Part Number: WL1831MOD Other Parts Discussed in Thread: WL1831 Hi, we know it should be possible to set up WL1831 as BLE master and thus allow simultaneous connection to multiple slaves at the same time.
But, is it possible the other way around? Maybe…