Part Number: WL1835MOD Other Parts Discussed in Thread: WL1835
Hi,
In our product, we use WL1835MODGB and have enabled both WiFi & BLE. My question is -
Do we need to get the end product BT SIG certified to be able to use the BT/BLE logo?
I don…
Hi FFatima,
You are correct that you would only have 31 bytes available in the advertisement packet, given that the WL18xx devices do not support BLE extended advertising. Yes, the flags should be included. However, the device could still respond to scan…
Hi Dylan,
sure my email is nicola.conforti@faro.com .
In need the certificado anatel referring to model WL18 MODGB (TEST GRADE: 31) which i believe is part of WL1835MOD. In any case the only part number available on TI website is WL1835MOD so i wrote down…
Part Number: WL1835MOD
Hi,
I am using Bluetopia 5.1 stack, currently the WiLink device would just be a non-connectable beacon but later on we will allow connection over GATT/SPP-LE profile.
Could you please answer the below questions:
I am interested…
Part Number: WL1835MOD Hi,
My customer is using WirelessTools-4.0.0.2 with WL1835MOD. However we were unable to locate the bin file "wl18xx-fw-4_MAC31_PHY224.bin" as detailed in the RTTT GUI. Can you kindly direct to the right link to download the bin…
Part Number: WL1835MOD Hi,
I think I have a problem with wl18xx problem
I am using beaglebone blue
[53233.855249] wlcore : ERROR SW watchdog interrupt received ! starting recovery .
[53233.862422] ------------ [ cut here ] ------------
[53233.862728] WAR…
Part Number: WL1835MOD I was asked to i nvestigate the ability for the Wi-Fi application (of my product) to integrate Wi-Fi channel hopping to optimize the different Wi-Fi bands incase of overcrowding.
For that I need to find out that if WL1835MOD chip…
Part Number: WL1835MOD Other Parts Discussed in Thread: WL1835 Hello ,
Yes , we talk about wilink8 driver for WL1835MOD on QNX for imx6.
The driver was availlable in QNX7.0 , but seem not be done for QNX 7.1.
The physical interface use by the driver…
Part Number: WL1835MOD Other Parts Discussed in Thread: WL1835
Hi,
Can you let me know which all features available in Bluetooth 5.1 specification is supported by WiLink 1835MODGB?
Regards
Fariya