Part Number: CC1310 Hi team,
The customer is designing a WM-Bus module based on CC1310 and WMBUS-CC13X0. The module will communicate with the customer's smart meter over UART.
The WM-Bus module collects data from nearby WM-Bus gas and water meters…
Part Number: LP-CC1312R7 Other Parts Discussed in Thread: WMBUS , , CC1312R7 , CC1101 , CC1200 Hi,
I have successfully performed rx measurements on Wmbus OTM sending packets either between 2 boards or between an ESG 4438C signal generator and a LP…
Part Number: CC1310 Other Parts Discussed in Thread: WMBUS Hi,team;
Using SDK: wmbus_ cc13x0_ rtos_ 2_ 0_ 0,T1_ C1 routine, change to 10S to send data once, and call wmbus_ apl_ setClock(); during initialization;
Set the system clock to local time…
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: WMBUS , CC1310 Hello forum
I want to create a wmbus application that can handle t1 and c1 modes on the cc1310 launchpad. I Have seen the stackforce implementation of the wmbus stack but i…
Part Number: LAUNCHXL-CC1350-4 Hi guys,
I use WMBUS API from https://www.ti.com/tool/WMBUS
I use a pair CC1350 for Meter and Collector. The other CC1350 for checking the status of WMBUS.
The API is woking in configuration "APL_CC13XX_Meter_T2_C2…
Part Number: CC1312R Other Parts Discussed in Thread: WMBUS Hi Champs,
Customer evaluates our WMBUS offer and has the following challenges:
"When I use partial mode for WMBUS (I finally used the non repeat mode RX, I have one RX cmd chained to a loop…
Part Number: CC1310 Other Parts Discussed in Thread: WMBUS , I'm working on a project based on EasyLinkEcho (RX/TX) example (SimpleLink CC13x0 SDK v4.20.02.07 in CCS 12.0.0.00009). In parallel I'm using wMBus stack (wmbus-cc13xx-rtos-2.0.0 in CCS 8.1…
Part Number: CC1310 Other Parts Discussed in Thread: WMBUS Hello,
I am having trouble talking to a third party device. I believe one possible cause is that the device may only support OMS v3.0.1. I notice that the WMBus stack adds the extended link…
Part Number: CC1310 Other Parts Discussed in Thread: WMBUS Hello,
I am debugging communication between the CC1310 Launchpad and a third party device. I have been running the APL Meter T1 example, and have exported the MCE_GPO0 signal to an external…
Part Number: CC1310 Other Parts Discussed in Thread: WMBUS Hi,
in a post around 5 years ago it is written that the wMBus patch also sends Postamble if using the patch as described in swra522 .
Related qustion: https://e2e.ti.com/support/wireless-connectivity…