Part Number: XIO1100 Dear team
It is a mass production project, currently line down because the detection issue, sometimes the system can not identify the PCIE device when power up.
so we would like to know, if there have some process to locate the root…
Part Number: XIO1100 HI
I want to used XIO1100 for my product , and the PC's PCI-E interface to my control borad. I used an ARM-M3 core platform, It couldn't support the 125MHz TI-PIPE MAC Interface.
Can I use a 50Mhz clock on the XIO1100's TX and…
Other Parts Discussed in Thread: XIO1100 For the XIO1100 chip, we have a non-working prototype board, and are uncertain what is the correct rotation for the XIO1100 chip on the PCB. The datasheet is useless in this regard. Which of the following four chip…
Other Parts Discussed in Thread: XIO1100 Can you send me (or post here) a schematic of a known good board which uses the XIO1100 chip? I am looking for a bit more detail than what is included in the datasheet.
Other Parts Discussed in Thread: XIO1100 We have a prototype board which uses the XIO1100ZGB chip, and said chip is so far showing no signs of life. Internet research indicates that this chip has a special startup sequence which has to be followed, and…
Other Parts Discussed in Thread: XIO1100 For the XIO1100, it is a shame that no real 3.3V JTAG port was included, especially given that such is part of the PCI Express interface, TI has been very active in JTAG testing, and there are so many parallel interface…
Other Parts Discussed in Thread: XIO1100 For the XIO1100 chip, we have a non-working prototype PCB. The XIO1100 has no RX_CLK output signal, even though it has 3.3V and 1.8V and 1.5V power, and the two REFCLK input signals are good (100MHz from PCI Express…
Other Parts Discussed in Thread: XIO1100 For the XIO1100 chip, we have a non-working prototype PCB, and urgently need to get it working. There are no signs of life yet from the XIO1100 chip. To help us debug the problem(s), which may be due to an incorrectly…
Other Parts Discussed in Thread: XIO1100 Hi,
I'm interest in XIO1100, as I need to use it as a PCIe to GPIO converter, I will connect its parallel I/Os to my controller, and interface its PCIe side to my PC, sorry but I'm new to PCIe interface and don…